IVIDDEC1_Status Struct Reference
[IVIDDEC1 - XDM Video Decoder Interface]

Defines instance status parameters. More...

#include <ividdec1.h>

Collaboration diagram for IVIDDEC1_Status:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 extendedError
XDM1_SingleBufDesc data
XDAS_Int32 outputHeight
XDAS_Int32 outputWidth
XDAS_Int32 frameRate
XDAS_Int32 bitRate
XDAS_Int32 contentType
XDAS_Int32 outputChromaFormat
XDM_AlgBufInfo bufInfo

Detailed Description

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.
All fields correspond to latest IVIDDEC1_Fxns::process() call on the particular instance of the decoder.
See also:
IVIDDEC1_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.

See also:
XDM_ErrorBit

Buffer descriptor for data passing.

Remarks:
If this field is not used, the application must set data.buf to NULL.
This buffer can be used as either input or output, depending on the command.
The buffer will be provided by the application, and returned to the application upon return of the IVIDDEC1_Fxns.control() call. The algorithm must not retain a pointer to this data.
See also:
XDM_GETVERSION

Output height in pixels.

Output width in pixels.

Average frame rate in fps * 1000. For example, if average frame rate is 30 frames per second, this field should be 30000.

Average bit rate, in bits per second.

Video content types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE

See also:
IVIDEO_ContentType

Chroma formats.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE

See also:
XDM_ChromaFormat

Input and output buffer information.

See also:
XDM_AlgBufInfo

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated