ISPHENC_InArgs Struct Reference
[ISPHENC - XDM Speech Encoder Interface]

Defines the input arguments for all ISPHENC instance process function. More...

#include <isphenc.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 nullTrafficChannel

Detailed Description

Defines the input arguments for all ISPHENC instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.
See also:
ISPHENC_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

1 = ON, 0 = OFF


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated