ISPHENC1_Params Struct Reference
[ISPHENC1 - XDM Speech Encoder Interface]

Defines the creation time parameters for all ISPHENC1 instance objects. More...

#include <isphenc1.h>

Data Fields

XDAS_Int16 size
XDAS_Int16 frameSize
XDAS_Int16 compandingLaw
XDAS_Int16 packingType
XDAS_Int16 vadSelection
XDAS_Int16 codecSelection
XDAS_Int16 bitRate
XDAS_Int16 reserved
XDAS_Int8 ** tablesPtr

Detailed Description

Defines the creation time parameters for all ISPHENC1 instance objects.

Remarks:
Some of the fields in this structure are optional and depend on the class of speech encoder you're creating.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Input frame size in bytes for sample based codecs.

Optional, codec-specific companding law. See your codec-specific interface documentation options.

See also:
ISPEECH1_PCM_CompandingLaw
ISPEECH1_G726_CompandingLaw

Optional, codec-specific packing type. See your codec-specific interface documentation options.

See also:
ISPEECH1_AMR_PackingType
ISPEECH1_G726_PackingType
ISPEECH1_WBAMR_PackingType

Optional, codec-specific voice activity detection selection. See your codec-specific interface documentation options.

See also:
ISPEECH1_AMR_VADSelect
ISPEECH1_SMV_VADSelect

Optional, codec-specific codec selection. See your codec-specific interface documentation options.

See also:
ISPEECH1_AMR_CodecSelect
ISPHENC1_Params.codecSelection

Optional, codec-specific bit rate. See your codec-specific interface documentation options.

See also:
ISPEECH1_AMR_BitRate
ISPEECH1_G723_BitRate
ISPEECH1_G726_BitRate
ISPEECH1_WBAMR_BitRate

Reserved - serves to pad this structure.

Optional pointer to the codec's initialization tables.

Remarks:
This parameter specifies a pointer to the array of the codec's table block pointers. If the application requires the codec to select the default table address array pointer, it should set this to NULL.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated