IAUDENC1_OutArgs Struct Reference
[IAUDENC1 - Audio Encoder Interface]

Defines the run time output arguments for all IAUDENC1 instance objects. More...

#include <iaudenc1.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 extendedError
XDAS_Int32 bytesGenerated
XDAS_Int32 numZeroesPadded
XDAS_Int32 numInSamples

Detailed Description

Defines the run time output arguments for all IAUDENC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.
See also:
IAUDENC1_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.

See also:
XDM_ErrorBit

Number of bytes generated during the process() call.

Number of zeroes padded to input.

Remarks:
Some of the encoders pad zeroes at the end of the stream to complete the last frame.

Number of input samples per channel consumed by the encoder.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated