IAUDENC1_InArgs Struct Reference
[IAUDENC1 - Audio Encoder Interface]

Defines the input arguments for all IAUDENC1 instance process function. More...

#include <iaudenc1.h>

Collaboration diagram for IAUDENC1_InArgs:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 numInSamples
XDM1_SingleBufDesc ancData

Detailed Description

Defines the input arguments for all IAUDENC1 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.
See also:
IAUDENC1_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Number of Input Samples per Channel.

See also:
IAUDENC_Params.inputBitsPerSample

Ancillary Data.

Remarks:
Ancillary data contains any extra information to be encoded along with the PCM samples.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated