IVIDANALYTICS_OutArgs Struct Reference
[IVIDANALYTICS - XDM Beta Video Analytics Interface]

Defines the run time output arguments for all IVIDANALYTICS instance objects. More...

#include <ividanalytics.h>

Collaboration diagram for IVIDANALYTICS_OutArgs:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 numTargets
XDM_Rect targets [128]
XDAS_Int32 numEvents
XDAS_Int32 eventId [128]
XDAS_Int32 extendedError
XDM_Date date

Detailed Description

Defines the run time output arguments for all IVIDANALYTICS instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.
See also:
IVIDDEC1_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Number of targets detected

target locations.

Remarks:
If numTargets is zero, the values in this array are undefined.

Number of events detected

Zero-terminated array containing the ids of rules fired during the process() call.

Remarks:
If numEvents is zero, the values in this array are undefined.

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.

See also:
XDM_ErrorBit

Current time.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated