![]() |
![]() |
Defines the creation time parameters for all IAUDDEC1 instance objects. More...
#include <iauddec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | outputPCMWidth |
XDAS_Int32 | pcmFormat |
XDAS_Int32 | dataEndianness |
Defines the creation time parameters for all IAUDDEC1 instance objects.
size
parameter. size
field must be correctly set by the caller. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Number of bits per output PCM Sample.
Output PCM Format Block/Interleaved.
Endianness of output data.