IAUDDEC - XDM Audio Decoder Interface

Data Structures

struct  IAUDDEC_Obj
 This must be the first field of all IAUDDEC instance objects. More...
struct  IAUDDEC_Params
 Defines the creation time parameters for all IAUDDEC instance objects. More...
struct  IAUDDEC_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  IAUDDEC_InArgs
 Defines the input arguments for all IAUDDEC instance process function. More...
struct  IAUDDEC_Status
 Defines instance status parameters (read-only). More...
struct  IAUDDEC_OutArgs
 Defines the run time output arguments for all IAUDDEC instance objects. More...
struct  IAUDDEC_Fxns
 Defines all of the operations on IAUDDEC objects. More...

Defines

#define IAUDDEC_CID   "ti.xdais.dm.IAUDDEC"
#define IAUDDEC_ERUNTIME   XDM_ERUNTIME
#define IAUDDEC_EOK   XDM_EOK
#define IAUDDEC_EFAIL   XDM_EFAIL

Typedefs

typedef struct IAUDDEC_ObjIAUDDEC_Handle
 Opaque handle to an IAUDDEC objects.
typedef IALG_Cmd IAUDDEC_Cmd
 Defines the control commands for the IAUDDEC module.

Detailed Description

This is the XDM IAUDDEC Audio Decoder Interface.

Deprecated:
This XDM audio decoder interface has been deprecated, and superceeded by newer IAUDDECx audio decoder interfaces.

Define Documentation

#define IAUDDEC_CID   "ti.xdais.dm.IAUDDEC"

IAUDDEC Class ID

#define IAUDDEC_ERUNTIME   XDM_ERUNTIME

General runtime failure.

#define IAUDDEC_EOK   XDM_EOK

Success.

#define IAUDDEC_EFAIL   XDM_EFAIL

General failure.


Typedef Documentation

typedef struct IAUDDEC_Obj* IAUDDEC_Handle

Opaque handle to an IAUDDEC objects.

Defines the control commands for the IAUDDEC module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IAUDDEC_Fxns::control()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated