ISPHENC_OutArgs Struct Reference
[XDM ISPHENC Speech/Voice Encoder Interface]

Defines the run time output arguments for all ISPHENC instance objects. More...

#include <isphenc.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 rate
XDAS_Int32 frameType
XDAS_Int32 outbufferSize

Detailed Description

Defines the run time output arguments for all ISPHENC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.
See also:
ISPHENC_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Current frame bit rate.

Current frame type.

Output buffer size in bytes.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated