Defines the run time output arguments for all IVIDTRANSCODE instance objects. More...
#include <ividtranscode.h>
Defines the run time output arguments for all IVIDTRANSCODE instance objects.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
Number of bits consumed during the IVIDTRANSCODE_Fxns.process() call.
Number of bits generated during the IVIDTRANSCODE_Fxns.process() call for each transcode output.
Type of the decoded picture.
Structure of the decoded picture.
Type of the encoded picture for each transcode output.
Structure of the encoded picture for each transcode output.
Decoded frame height
Decoded frame width
This is the ID of the encoded buffer for each output. This field is also used by the client to identify the outBufs
supplied with the IVIDTRANSCODE_Fxns.process() call that can be reused.
Flag to indicate if the current frame was skipped in specific transcode outputs.
When outputID
for a specific transcode output is non-zero, the corresponding encoded buffer related information is populated here.
Flag to indicate that the outBufs
provided with the IVIDTRANSCODE_Fxns.process() call are in use. No outBufs are required to be supplied with the next IVIDTRANSCODE_Fxns.process() call.