Defines the input arguments for all IVIDDEC instance process function. More...
#include <ividenc.h>
Data Fields | |
XDAS_Int32 | size |
Defines the input arguments for all IVIDDEC instance process function.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.