Defines the creation time parameters for all IVIDENC1 instance objects. More...
#include <ividenc1.h>
Defines the creation time parameters for all IVIDENC1 instance objects.
size
parameter. size
field must be correctly set by the caller. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Encoding preset.
Video rate control presets.
Maximum video height in pixels.
Maximum video width in pixels.
Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.
Maximum bit rate, bits per second.
Endianness of output data.
I to P frame distance. e.g. = 1 if no B frames, 2 to insert one B frame.
Chroma format for the input buffer.
Video content type of the buffer being encoded.
Chroma formats for the reconstruction buffers.