Defines the run time output arguments for all ISPHDEC instance objects. More...
#include <isphdec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | mode |
Defines the run time output arguments for all ISPHDEC instance objects.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Speech voice mode. See ISPEECH_VoiceMode.