This structure defines the codec parameters that can be modified after creation via control() calls. More...
#include <iauddec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | downSampleSbrFlag |
This structure defines the codec parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Flag to indicate downsampling for SBR.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.