IRES

Data Structures

struct  IRES_YieldContext
 Specifies the algorithm specific handles and context save & restore function pointers and arguments that the framework will call during a context switch. More...
struct  IRES_Fxns
 These fxns are used to query/grant the resources requested by the algorithm at initialization time, and to change these resources at runtime. All these fxns are implemented by the algorithm, and called by the client of the algorithm. More...

Typedefs

typedef Void(* IRES_ContextSaveFxn )(IALG_Handle algHandle, Void *contextArgs)
typedef Void(* IRES_ContextRestoreFxn )(IALG_Handle algHandle, Void *contextArgs)
typedef IRES_YieldContextIRES_YieldContextHandle
typedef Void * IRES_YieldArgs
typedef Void(* IRES_YieldFxn )(IRES_YieldResourceType resourceType, IRES_YieldContextHandle algYieldContext, IRES_YieldArgs yieldArgs)
 The 'yield function' pointer and 'yield arguments' are supplied to an algorithm during its IRES interface 'initialization'. The algorithm optionally calls the yield function during its 'process' stages for co-operative multi-tasking and pre-emption by a higher priority algorithm.

Enumerations

enum  IRES_YieldResourceType {
  IRES_ALL = 0,
  IRES_SCRATCHMEMORY,
  IRES_SCRATCHDMA,
  IRES_RESOURCEHANDLE
}



enum  IRES_Status {
  IRES_OK = 0,
  IRES_EALG = 1,
  IRES_EEXISTS = 2,
  IRES_EFAIL = 3,
  IRES_EINIT = 4,
  IRES_ENOINIT = 5,
  IRES_ENOMEM = 6,
  IRES_ENORESOURCE = 7,
  IRES_ENOTFOUND = 8
}
 

IRES_Status defines the standard error and success codes returned by IRES APIs.

More...
enum  IRES_RequestMode {
  IRES_SCRATCH,
  IRES_PERSISTENT,
  IRES_LATEACQUIRE
}
 

Mode in which resources can be requested.

More...
typedef struct IRES_ObjIRES_Handle
 Handle to "logical" resource.

Detailed Description

The IRES interface enables algorithms to request and receive handles representing private logical resources.


Typedef Documentation

typedef Void(* IRES_ContextSaveFxn)(IALG_Handle algHandle, Void *contextArgs)
typedef Void(* IRES_ContextRestoreFxn)(IALG_Handle algHandle, Void *contextArgs)
typedef Void* IRES_YieldArgs
typedef Void(* IRES_YieldFxn)(IRES_YieldResourceType resourceType, IRES_YieldContextHandle algYieldContext, IRES_YieldArgs yieldArgs)

The 'yield function' pointer and 'yield arguments' are supplied to an algorithm during its IRES interface 'initialization'. The algorithm optionally calls the yield function during its 'process' stages for co-operative multi-tasking and pre-emption by a higher priority algorithm.

An operating system level context switch may occur during the yield call. Whenever a context switch occurs, all scratch resources owned by the yielding algorithm must be context saved prior to the context switch and restored and initialized prior to 'resumption' by the framework/application. The 'yielding' algorithm must supply the IRES_YieldContext and the 'yield arguments' it received during IRES initialization. The framework calls the context save & restore functions provided by the yielding algorithm's IRES_YieldContext.

typedef struct IRES_Obj* IRES_Handle

Handle to "logical" resource.


Enumeration Type Documentation

Enumerator:
IRES_ALL 

Yielding all resources held by the algorithm.

IRES_SCRATCHMEMORY 

Yielding all scratch memory resources held by the algorithm.

IRES_SCRATCHDMA 

Yielding all IDMA3 resources held by the algorithm.

IRES_RESOURCEHANDLE 

Yielding IRES resource handle only.

IRES_Status defines the standard error and success codes returned by IRES APIs.

Enumerator:
IRES_OK 

Success

IRES_EALG 

Error in algorithm IRES_Fxns functions

IRES_EEXISTS 

Error, already exists

IRES_EFAIL 

Generic Error Message

IRES_EINIT 

Error, already initialized

IRES_ENOINIT 

Error, not initialized

IRES_ENOMEM 

Error, not enough memory

IRES_ENORESOURCE 

Error, resource unavailable

IRES_ENOTFOUND 

Error, not found

Mode in which resources can be requested.

Enumerator:
IRES_SCRATCH 

Indicates that resource requested can be shared with other algorithms in the same group.

IRES_PERSISTENT 

Indicates that resource requested for allocation exclusively for this algorithm.

IRES_LATEACQUIRE 

Indicates that resource requested will not be granted immediately, but afterwards. Specific IRES APIs will need to be called, to ensure that a particular algorithm is the only user of these resources.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated