#include <ividenc1.h>
size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | inputID |
XDAS_Int32 | topFieldFirstFlag |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Identifier to attach with the corresponding encoded bitstream frames.
When there is no re-ordering, IVIDENC1_OutArgs::outputID will be the same as this inputID field.
Zero (0) is not a supported inputID. This value is reserved for cases when there is no output buffer provided.
Flag to indicate the field order in interlaced content.
This field is only applicable to the input image buffer.
This field is only applicable for interlaced content, not progressive.