#include <iauddec1.h>
size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
XDAS_Int32 | bytesConsumed |
XDAS_Int32 | numSamples |
XDAS_Int32 | channelMode |
XDAS_Int32 | lfeFlag |
XDAS_Int32 | dualMonoMode |
XDAS_Int32 | sampleRate |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.
Number of bytes consumed during the process() call.
Number of output samples per channel.
Flag indicating the precense of LFE channel in the output. When the LFE channel is not in the output, this is set to XDAS_FALSE.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
Mode to indicate type of Dual Mono. Only used in case of Dual Mono output.
Sampling frequency, in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.