XDAIS 6.24 Release Notes
May 2009
Introduction,
Documentation,
What's New,
Upgrade Info,
Compatibility Information,
Validation Info,
Known Issues,
Examples,
Version Information,
Technical Support.
This XDAIS product contains the DSP Algorithm Interface Standard specification
and related documentation and examples.
The following packages are included in this release:
-
ti.xdais - XDAIS interface and documentation
-
ti.xdais.dm - XDAIS-DM (XDM) interface and
documentation.
-
ti.xdais.qualiti - XDAIS compliancy checking tool
In addition several example packages are also provided.
The following documentation is available:
In addition, users are encouraged to monitor (and contribute to!) the
TI Embedded Processors Wiki.
Release notes from previous releases are also available in the relnotes_archive directory.
The following significant changes have been made since 5.00
6.24 (This Release)
- New features
- QualiTI improvements
- Validated examples against WinCE targets
- The following defects were resolved:
- The following enhancements were resolved:
6.23
- New features
- QualiTI enhancements to include ARM support
- The following defects were resolved:
ID |
Headline |
SDOCM00053259 |
chm API Reference Guide search doesn't work
|
SDOCM00054295 |
QualiTI fails on Windows if the tool paths contain spaces
|
- The following enhancements were resolved:
ID |
Headline |
SDOCM00054214 |
Add 674 target support to QualiTI
|
SDOCM00054216 |
Add QualiTI -g option to support launching GUI with a given filename
|
6.22
- New features
- Added new chroma formats to XDM_ChromaFormat enum
- The following enhancements were resolved:
ID |
Headline |
SDSCM00050966 |
Add more Chroma format enums |
6.21
- New features
- The following enhancements were resolved:
ID |
Headline |
SDOCM00049826 |
Change Licensing to BSD |
SDOCM00050452 |
Add the ability for extending XDM-defined enums |
6.20
- New features
- Documentation updates, including error resiliency clarifications
in IVIDDEC2.
- Minor bug fixes in QualiTI.
- Changes to IVIDANALYTICS API in response to customer feedback. This
breaks compatibility with previous releases of IVIDANALYTICS, but the
API continues to be in Beta form and therefore changable.
- The following defects were resolved:
ID |
Headline |
SDSCM00024690 |
QualiTI doesn't catch not-an-archive Rule 15 if in an XDC package |
SDSCM00025188 |
QualiTI needs to handle _IALG symbols when they're const |
SDSCM00025559 |
viddec2_copy example has incorrect symbol in header |
- The following enhancements were resolved:
ID |
Headline |
SDSCM00024172 |
Examples which use package.bld should have explicit Build and Pkg assignments |
SDSCM00025558 |
IVIDDEC2 spec should state that valid bufs can be returned when non-fatal EFAIL is returned from process() |
SDSCM00026170 |
Add IUNIVERSAL to XDM spec |
6.00
- Introduction of IRES interfaces.
- Introduction of the video transcoder APIs (IVIDTRANSCODE)
- Introduction of video analytics Beta APIs (IVIDANALYTICS).
These APIs are available for review, and will be replaced with the
final interfaces in a future release.
- Deprecated XDM 0.9 interfaces. These interfaces are fully supported in
this release, but support will be removed in a future release. XDM algorithm
producers are strongly encouraged to migrate to the XDM 1.00 interfaces.
- Updated ti.xdais.dm.examples.g711 codec package to include
G.711 decode support and both u-law and a-law transforms.
5.21
- Official release of XDM 1.00. Examples and API Reference Guides
have been updated accordingly.
- And the following MRs were resolved:
ID |
Headline |
SDSCM00014553 |
Remove dependency on BIOS types in idma3.h |
SDSCM00013817 |
Deprecate XDM_ERUNTIME for XDM 1.00 |
SDSCM00013698 |
Add bitrate fields to several speech1 structs and more frame
types |
SDSCM00013621 |
XDM 1.0 speech inArgs should have "size" field for extensibility |
SDSCM00013568 |
XDM user guide needs to discuss extension of parameter ad
argument structions |
SDSCM00013537 |
ISPHENC1_FrameType enums have inconsistant prefix |
SDSCM00011273 |
When including public header files in XDAIS, one needs to
use "full qualified package path" |
SDSCM00005724 |
XDAIS Documentation needs to be update to support IDMA3 |
5.10
- Introduction of XDM 1.00 Beta.
- The Reference Guide has been updated to include these Beta
APIs.
- Added "What's New in XDM
1.00" documentation, describing the high-level changes in the
XDM 1.00 Beta specification.
- This XDM 1.00 Beta spec addresses the following items:
- SDSCM00004685 - XDM speech enc and dec OutArgs should
have extendedError field for consistency
- SDSCM00005009 - IIMGDEC_OutArgs bytesconsumed should be
camelCase
- SDSCM00005245 - Video enc interface needs to reconsider
reconBufs conventions for RPCs
- Addition of example "copy" codecs, conforming with XDM 1.00 Beta
interfaces.
- Addition of example G.711 algorithm, conforming with XDM 0.90
speech encoder interface. This example shows how to wrap an XDM
interface around an existing algorithm.
- Addition of example "extended" video encoder copy codec. This
example shows how an algorithm can extend the XDM interface to
implement codec-specific features.
- SDSCM00005726 - Add doxygen comments to ialg.h
- SDSCM00005728 - IDMA3 channel object documentation needs to
include scratch environment support
- SDSCM00010925 - XDM User's manual uses XMI in places
- SDSCM00011274 - XDAIS header files for c55 need to include fully
qualified package files
The XDAIS packages are available in the "packages/"
subdirectory of the product. If you have a previous release of the
XDAIS product, you can install this release next to it, and
modify your builds to use this newer release.
If you're using the DVEVM, this can be done by setting the
XDAIS_INSTALL_DIR variable in the Rules.make file at the
top of the DVEVM distribution directory.
Compatibility Breaks!
None
Note, if you're upgrading from a release earlier than XDAIS 6.23, be
sure to review the Upgrade section for each of the releases between
your current XDAIS release and this one. Previous release notes are
available in the relnotes_archive directory.
The details provided below describe each package's compatibility with the
previous release (6.23).
-
ti.xdais - This package is compatible with the
previous release. (Compatibility key: 1,2.0,1 -> 1,2.0,1)
-
ti.xdais.dm - This package is compatible with
the previous release. (Compatibility key: 1,0,5 -> 1,0,5)
-
Compatibility with previous releases is not currently managed in
the examples.
If migrating from a release prior to XDAIS 6.23, consult previous
releases available in the relnotes_archive directory.
Compatibility Key Definitions
Compatibility keys are intentionally independent of Marketing product
numbers and are intended to:
- Enable tooling to identify incompatibilities between components,
and
- Convey a level of compatibility between different releases to
set end user expectations.
Compatibility keys are composed of 3 comma-delimited numbers - M,S,R
- where:
- M = Major. A difference in M indicates a break in
compatibility.
- S = Source. A difference in S indicates source
compability. That is, the user's source doesn't require change, but
does require rebuilding.
- R = Radix. A difference in R indicates an introduction
of new features, but compatibility with previous interfaces has not
broken. If libraries are provided by the package, an application
must re-link with the new libraries, but not rebuild from source.
This release was validated against using the following components:
- XDC Tools 3.10.05.61
- The examples were built with the following toolchains. Note
that, in general, nothing prevents them from being built with a
different version of tools, nor for other devices - they are
intentionally written in generic C):
- gnu.targets.Linux86 - 4.1.0
- gnu.targets.UCArm9 - 4.2.1
- gnu.targets.arm.GCArmv5T - 4.2.1
- microsoft.targets.arm.WinCE - 14.01.60511
- ti.targets.C28_large - 5.1.2
- ti.targets.C55P_byte - 4.0.0
- ti.targets.C55_huge - 3.2.2
- ti.targets.C55_large - 3.2.2
- ti.targets.C64P - 6.0.16
- ti.targets.C674 - 6.1.5
- QualiTI
- Rule 15 - Each XDAIS-compliant algorithm must be packaged in an
archive which has a name that follows a uniform naming convention - has
been disabled.
XDAIS examples and instructions are located in the
"examples" directory.
This product's version follows a version format, M.mm.pp.bb,
where M is a single digit Major number, mm is 2 digit
minor number, pp is a 2 digit patch number, and b is an
unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the
product version is encoded in the top level directory,
ex. xdais_6_24.
Subsequent releases of patch upgrades will be identified by the patch
number, ex. XDAIS 6.24.01 with directory xdais_6_24_01.
Typically, these patches only include critical bug fixes.
For technical support, contact softwaresupport@ti.com
Check the following web site for updates: https://www-a.ti.com/downloads/sds_support/targetcontent/XDAIS/index.html
Last updated: May 27, 2009