#include <ividdec1.h>
size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numBytes |
XDAS_Int32 | inputID |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Size of input data in bytes, provided to the algorithm for decoding.
The decoder will attach this ID with the corresponding output frames.
When there is no re-ordering, IVIDDEC1_OutArgs::outputID will be same as this inputID field.
Zero (0) is not a supported inputID. This value is reserved for cases when there is no output buffer provided in IVIDDEC1_OutArgs::displayBufs.