#include <ialg.h>
Data Fields | |
Void * | implementationId |
Unique pointer that identifies the module implementing this interface. | |
Void(* | algActivate )(IALG_Handle handle) |
Notification to the algorithm that its memory is "active" and algorithm processing methods may be called. | |
Int(* | algAlloc )(const IALG_Params *params, struct IALG_Fxns **parentFxns, IALG_MemRec *memTab) |
Apps call this to query the algorithm about its memory requirements. Must be non-NULL. | |
Int(* | algControl )(IALG_Handle handle, IALG_Cmd cmd, IALG_Status *status) |
Algorithm specific control and status. | |
Void(* | algDeactivate )(IALG_Handle handle) |
Save all persistent data to non-scratch memory. | |
Int(* | algFree )(IALG_Handle handle, IALG_MemRec *memTab) |
Apps call this to allow the algorithm to initialize memory requested via algAlloc(). Must be non-NULL. | |
Int(* | algInit )(IALG_Handle handle, const IALG_MemRec *memTab, IALG_Handle parent, const IALG_Params *params) |
Initialize an algorithm's instance object. Must be non-NULL. | |
Void(* | algMoved )(IALG_Handle handle, const IALG_MemRec *memTab, IALG_Handle parent, const IALG_Params *params) |
Notify algorithm instance that instance memory has been relocated. | |
Int(* | algNumAlloc )(Void) |
Number of memory allocation requests required. |
Unique pointer that identifies the module implementing this interface.
Void(* IALG_Fxns::algActivate)(IALG_Handle handle) |
Notification to the algorithm that its memory is "active" and algorithm processing methods may be called.
[in] | handle | Handle to an algorithm instance. |
The implementation of algActivate() (and algDeactivate()) is required if the algorithm requests memory of type IALG_SCRATCH.
The algActivate() method should only be implemented if a module wants to factor out initialization code that can be executed once prior to processing multiple consecutive frames of data.
If a module does not implement this method, the algActivate() field in the module's static function table (of type IALG_Fxns) must be set to NULL
. This is equivalent to the following implementation:
Void algActivate(IALG_Handle handle) { }
handle
must be a valid handle for the algorithm's instance object.
No other algorithm method is currently being run on this instance. This method never preempts any other method on the same instance.
If the algorithm has implemented the IDMA2 interface, algActivate() can only be called after a successful return from dmaInit().
Int(* IALG_Fxns::algAlloc)(const IALG_Params *params, struct IALG_Fxns **parentFxns, IALG_MemRec *memTab) |
Apps call this to query the algorithm about its memory requirements. Must be non-NULL.
[in] | params | Algorithm specific attributes. |
[out] | parentFxns | Parent algorithm functions. |
[out] | memTab | array of memory records. |
If algNumAlloc() is not implemented, the maximum number of initialized memory records is IALG_DEFMEMRECS.
The first argument to algAlloc() is a pointer to the creation parameters for the instance of the algorithm object to be created. This pointer is algorithm-specific; i.e., it points to a structure that is defined by each particular algorithm. This pointer may be NULL
; however, in this case, algAlloc() must assume default creation parameters and must not fail.
The second argument to algAlloc() is an optional parameter. algAlloc() may return a pointer to its parent's IALG functions. If this output value is assigned a non-NULL value, the client must create the parent instance object using the designated IALG functions pointer. The parent instance object must then be passed to algInit().
algAlloc() may be called at any time and it must be idempotent; i.e., it can be called repeatedly without any side effects, and always returns the same result.
memTab
[] is no less than the number returned by algNumAlloc().
*parentFxns
is a valid pointer to an IALG_Fxns pointer variable.
*parentFxns
is set to a non-NULL value that points to a valid IALG_Fxns structure, the parent's IALG implementation. Otherwise, this pointer is not set. algAlloc() may elect to ignore the parentFxns
pointer altogether.
For each memory descriptor in memTab with an IALG_WRITEONCE attribute, the algorithm has either set the base field to a non-NULL value, which is the address of a statically allocated and initialized memory buffer of the indicated 'size', or has set the base field to NULL
, thereby requiring the memory for the buffer to be provided by the client.
Exactly
elements of the memTab
[] array are initialized, where n
is the return value from this operation.
For each memory descriptor in memTab
with an IALG_PERSIST or IALG_SCRATCH attribute, the algorithm does not set its base field.
memTab
[0] defines the memory required for the instance's object and this object's first field is an IALG_Obj structure.
memTab
[0] is requested as persistent memory.
Int(* IALG_Fxns::algControl)(IALG_Handle handle, IALG_Cmd cmd, IALG_Status *status) |
Algorithm specific control and status.
[in] | handle | Algorithm instance handle. |
[in] | cmd | Algorithm specific command. |
[out] | status | Algorithm specific status. |
cmd
, and an input/output status buffer pointer to an algorithm's instance object.In preemptive execution environments, algControl() may preempt a module's other metods (for example, its processing methods).
The implementation of algControl() is optional. If a module does not implement this method, the algControl() field in the module's static function table (of type IALG_Fxns) must be set to NULL
. This is equivalent to the following implementation:
Void algControl(IALG_Handle handle, IALG_Cmd cmd, IALG_Status *status) { return (IALG_EFAIL); }
handle
must be a valid handle for the algorithm's instance object.
Algorithm specific cmd
values are always less than IALG_SYSCMD.
cmd
value is not recognized by the algorithm, the return value is not equal to IALG_EOK.Void(* IALG_Fxns::algDeactivate)(IALG_Handle handle) |
Save all persistent data to non-scratch memory.
[in] | handle | Algorithm instance handle. |
handle
is used by the algorithm to identify the various buffers that must be saved prior to the next cycle of algActivate() and processing.
The implementation of algDeactivate() (and algActivate()) is required if the algorithm requests memory of type IALG_SCRATCH.
The algDeactivate() method is only implemented if a module wants to factor out initialization code that can be executed once prior to processing multiple consecutive frames of data.
If a module does not implement this method, the algDeactivate() field in the module's static function table (of type IALG_Fxns) must be set to NULL
. This is equivalent to the following implementation:
Void algDeactivate(IALG_Handle handle) { }
The instance object is currently "active"; i.e., all instance memory is active and if an algActivate() method is defined, it has been called.
handle
must be a valid handle for the algorithm's instance object.
No other algorithm method is currently being run on this instance. This method never preempts any other method on the same instance.
All instance scratch memory may be safely overwritten.
Int(* IALG_Fxns::algFree)(IALG_Handle handle, IALG_MemRec *memTab) |
Apps call this to allow the algorithm to initialize memory requested via algAlloc(). Must be non-NULL.
[in] | handle | Algorithm instance handle. |
[out] | memTab | Output array of memory records. |
handle
. This function always returns a positive non-zero value indicating the number of records initialized. This function can never initialize more memory records than the value returned by algNumAlloc().memTab
[] array contains at least algNumAlloc() records.
handle
must be a valid handle for the algorithm's instance object.
If the prior call to algAlloc() returned a non-NULL parent functions pointer, then the parent instance must be an active instance object created via that function pointer.
No other agorithm method is currently being run on this instance. This method never preempts any other method on the same instance.
memTab
[] contains pointers to all of the memory passed to the algorithm via algInit().The size and alignment fields contain the same values passed to the client via algAlloc(); i.e., if the client makes changes to the values returned via algAlloc() and passes these new values to algInit(), the algorithm is not responsible for retaining any such changes.
Int(* IALG_Fxns::algInit)(IALG_Handle handle, const IALG_MemRec *memTab, IALG_Handle parent, const IALG_Params *params) |
Initialize an algorithm's instance object. Must be non-NULL.
[in] | handle | Algorithm instance handle. This is a pointer to an initialized IALG_Obj structure. Its value is identical to the memTab[0].base . |
[in] | memTab | Array of allocated buffers. |
[in] | parent | Handle of algorithm's parent instance. |
[in] | params | Pointer to algorithm's instance parameters. |
handle
is a pointer to an initialized IALG_Obj structure. Its value is identical to the memTab[0].base
.
memTab
is a table of memory records that describe the base address, size, alignment, type, and memory space of all buffers allocated for an algorithm instance (including the algorithm's instance object itself). The number of initialized records is identical to the number returned by a prior call to algAlloc().
parent
is a handle to another algorithm instance object. This parameter is often NULL; indicating that no parent object exists. This parameter allows clients to create a shared algorithm instance object and pass it to other algorithm instances. For example, a parent instance object might contain global read-only tables that are used by several instances of a vocoder.
params
is a pointer to algorithm-specific parameters that are necessary for the creation and initialization of the instance object. This pointer points to the same parameters passed to the algAlloc() operation. However, this pointer may be NULL. In this case, algInit(), must assume default creation parameters.
The algorithm must not access any scratch resources, memory or otherwise, until it has been activated (see algActivate()). A common error is to initialize scratch resources during algInit(). This is an error as another algorithm, or instance of the same algorithm, may be active when this instance's algInit() is called. This algorithm must not access scratch resources until it is active.
The client is not required to satisfy the IALG_MemSpace attribute of the requested memory. Note however that C6000 algorithms that use DMA may strictly require the client to satisfy its on-chip memory requirements and may not function correctly otherwise.
The client may allocate the requested IALG_WRITEONCE buffers once (or never, if the algorithm has assigned a base address in the prior call to algAlloc) and use the same buffers to initialize multiple instances of the same algorithm that are created with identical parameters.
typedef struct EncoderObj { IALG_Obj ialgObj; int workBuf; Int workBufLen; ... ; } EncoderObj; Int algInit(IALG_Handle handle, IALG_MemRec memTab[], IALG_Handle parent, IALG_Params *params) { EncoderObj *inst = (EncoderObj *)handle; EncoderParams *encParams = (EncoderParams *)params; if (encParams == NULL) { encParams = MYDEFAULTPARAMS; } inst->workBuf = memTab[1].base; inst->workBufLen = encParams->frameDuration * 8; ... return (IALG_EOK); }
memTab
contains pointers to non-overlapping buffers with the size and alignment requested via a prior call to algAlloc(). In addition, the algorithm parameters, params, passed to algAlloc() are identical to those passed to this operation.
handle
must be a valid handle for the algorithm's instance object; i.e., handle == memTab[0].base
and handle->fxns
is initialized to point to the appropriate IALG_Fxns structure.
If the prior call to algAlloc() has not assigned a non-NULL base address to an IALG_WRITEONCE memTab
entry, the client must provide the memory resource with the requested size and alignment.
If the prior call to algAlloc() returned a non-NULL parent functions pointer, then the parent handle, parent
, must be a valid handle to an instance object created via that function pointer.
No other algorithm method is currently being run on this instance. This method never preempts any other method on the same instance.
If parent
is non-NULL, no other method is currently being run on the parent instance; i.e., this method never preempts any other method on the parent instance.
If the prior call to algAlloc() assigned a non-NULL base address to an IALG_WRITEONCE memTab
[] entry, the client may pass back the same address in the base field without allocating additional memory for that persistent write-once buffer. Alternatively, the client may treat IALG_WRITEONCE buffers in the same way as IALG_PERSIST buffers; by allocating new memory and granting it to the algorithm using the base field.
The buffer pointed to in memTab
[0] is initialized with a pointer to the appropriate IALG_Fxns structure followed by all 0s.
All subsequent memory accesses to the IALG_WRITEONCE buffers by this algorithm instance will be read-only.
If the algorithm has implemented the IDMA2 interface, the dmaGetChannels() operation can be called.
Void(* IALG_Fxns::algMoved)(IALG_Handle handle, const IALG_MemRec *memTab, IALG_Handle parent, const IALG_Params *params) |
Notify algorithm instance that instance memory has been relocated.
[in] | handle | Algorithm instance handle. |
[in] | memTab | Array of allocated buffers. |
[in] | parent | Handle of algorithm's parent instance. |
[in] | params | Pointer to algorithm's instance parameters. |
The implementation of algMoved() is optional. However, it is highly recommended that this method be implemented. If a module does not implement this method, the algMoved() field in the module's static function table (of type IALG_Fxns) must be set to NULL
. This is equivalent to asserting that the algorithm's instance objects cannot be moved.
Int(* IALG_Fxns::algNumAlloc)(Void) |
Number of memory allocation requests required.
algNumAlloc() is optional; if it is not implemented, the maximum number of memory records for algAlloc() is assumed to be IALG_DEFMEMRECS. This is equivalent to the following implementation:
Void algNumAlloc(Void) { return (IALG_DEFNUMRECS); }
If a module does not implement this method, the algNumAlloc() field in the module's static function table (of type IALG_Fxns) must be set to NULL
.
#define NUMBUF 3 extern IALG_Fxns *subAlg; Int algNumAlloc(Void) { return (NUMBUF + subAlg->algNumAlloc()); } Int algAlloc(const IALG_Params *p, struct IALG_Fxns **pFxns, IALG_MemRec memTab) { Int n; ... n = subAlg->algAlloc(0, memTab); return (n + NUMBUF); }