XDM_ContextInfo Struct Reference
[Shared XDM Definitions]

#include <xdm.h>


Detailed Description

Buffer information descriptor for input and output buffers.


Data Fields

XDAS_Int32 minContextSize
XDAS_Int32 minIntermediateBufSizes [32]


Field Documentation

XDAS_Int32 XDM_ContextInfo::minContextSize

Minimum size, in 8-bit bytes, required for the alg context.

XDAS_Int32 XDM_ContextInfo::minIntermediateBufSizes[32]

Minimum size, in 8-bit bytes, required for each intermediate buffer.

Remarks:
The codec indicates the number of intermediate buffers required by zero-terminating this array.


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated