IVIDEO1_BufDesc Struct Reference
[XDM Video Interface]

#include <ivideo.h>

Collaboration diagram for IVIDEO1_BufDesc:

Collaboration graph
[legend]

Detailed Description

Detailed buffer descriptor for video buffers.


Data Fields

XDAS_Int32 numBufs
XDAS_Int32 frameWidth
XDAS_Int32 frameHeight
XDAS_Int32 framePitch
XDM1_SingleBufDesc bufDesc [3]
XDAS_Int32 extendedError
XDAS_Int32 frameType
XDAS_Int32 topFieldFirstFlag
XDAS_Int32 repeatFirstFieldFlag
XDAS_Int32 frameStatus
XDAS_Int32 repeatFrame
XDAS_Int32 contentType
XDAS_Int32 chromaFormat


Field Documentation

XDAS_Int32 IVIDEO1_BufDesc::numBufs

Number of buffers in bufDesc[].

XDAS_Int32 IVIDEO1_BufDesc::frameWidth

Width of the video frame.

XDAS_Int32 IVIDEO1_BufDesc::frameHeight

Height of the video frame.

XDAS_Int32 IVIDEO1_BufDesc::framePitch

Frame pitch used to store the frame.

Remarks:
This field can also be used to indicate the padded width.

XDM1_SingleBufDesc IVIDEO1_BufDesc::bufDesc[3]

Picture buffers.

XDAS_Int32 IVIDEO1_BufDesc::extendedError

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)

The value of each enum is the bit which is set.

Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.

The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.

This enumeration data type should not be used for storage, but rather only for its constant values.

See also:
XDM_ErrorBit

XDAS_Int32 IVIDEO1_BufDesc::frameType

Video frame types.

Remarks:
For the various IVIDEO_xy_FRAME values, this frame type is interlaced where both top and bottom fields are provided in a single frame. The first field is an "x" frame, the second field is "y" field.

This enumeration data type should not be used for storage, but rather only for its constant values.

This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.

See also:
XDM_CUSTOMENUMBASE

See also:
IVIDEO_FrameType

XDAS_Int32 IVIDEO1_BufDesc::topFieldFirstFlag

Flag to indicate when the application should display the top field first.

Remarks:
Valid values are XDAS_TRUE and XDAS_FALSE.

This field is only applicable for interlaced content, not progressive.

This field does not apply to encoder recon bufs.

XDAS_Int32 IVIDEO1_BufDesc::repeatFirstFieldFlag

Flag to indicate when the first field should be repeated.

Remarks:
Valid values are XDAS_TRUE and XDAS_FALSE.

This field is only applicable for interlaced content, not progressive.

This field does not apply to encoder recon bufs.

XDAS_Int32 IVIDEO1_BufDesc::frameStatus

Video output buffer status.

Remarks:
Ownership of the buffers, either by application or algorithm, is conveyed via these values.

This reflects the status of ALL output buffers. For example, if video decoded output is in 4:2:0 format, all the 3 output buffers' status is described by this value. Similarly, for 4:2:2 formatted buffers, this value describes the single buffer's status.

This enumeration data type should not be used for storage, but rather only for its constant values.

This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.

See also:
XDM_CUSTOMENUMBASE

See also:
IVIDEO_OutputFrameStatus
Remarks:
This field does not apply to encoder recon bufs.

XDAS_Int32 IVIDEO1_BufDesc::repeatFrame

Number of times the display process needs to repeat the displayed progressive frame.

Remarks:
This information is useful for progressive content when the decoder expects the display process to repeat the displayed frame for a certain number of times. This is useful for pulldown (frame/field repetition by display system) support where the display frame rate is increased without increasing the decode frame rate.

The default value is 0.

This field does not apply to encoder recon bufs.

XDAS_Int32 IVIDEO1_BufDesc::contentType

Content type of the buffer.

Remarks:
This is useful when the content is both interlaced and progressive. The display process can use this field to determine how to render the display buffer.
See also:
IVIDEO_ContentType

XDAS_Int32 IVIDEO1_BufDesc::chromaFormat

Chroma formats.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.

This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.

See also:
XDM_CUSTOMENUMBASE

See also:
XDM_ChromaFormat


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated