IVIDDEC_Params Struct Reference
[XDM IVIDDEC Video Decoder Interface]

#include <ividdec.h>


Detailed Description

Defines the creation time parameters for all IVIDDEC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.

This structure may be extended by individual codec implementation allowing customization with vendor specific parameters.

The size field must be correctly set by the caller.


Data Fields

XDAS_Int32 size
XDAS_Int32 maxHeight
XDAS_Int32 maxWidth
XDAS_Int32 maxFrameRate
XDAS_Int32 maxBitRate
XDAS_Int32 dataEndianness
XDAS_Int32 forceChromaFormat


Field Documentation

XDAS_Int32 IVIDDEC_Params::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

XDAS_Int32 IVIDDEC_Params::maxHeight

Maximum video height in pixels.

XDAS_Int32 IVIDDEC_Params::maxWidth

Maximum video width in pixels.

XDAS_Int32 IVIDDEC_Params::maxFrameRate

Maximum frame rate in fps * 1000.

XDAS_Int32 IVIDDEC_Params::maxBitRate

Maximum bit rate, bits per second. For example, if bit rate is 10 Mbps, set this field to 10000000

XDAS_Int32 IVIDDEC_Params::dataEndianness

Endianness of input data.

See also:
XDM_DataFormat

XDAS_Int32 IVIDDEC_Params::forceChromaFormat

Force decode in given Chroma format.

See also:
XDM_ChromaFormat


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated