IVIDANALYTICS_Params Struct Reference
[XDM Beta Video Analytics Interface]

#include <ividanalytics.h>


Detailed Description

Defines the creation time parameters for all IVIDANALYTICS instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.

The size field must be correctly set by the caller.


Data Fields

XDAS_Int32 size
XDAS_Int32 maxHeight
XDAS_Int32 maxWidth
XDAS_Int32 maxFrameRate
XDAS_Int32 dataEndianness
XDAS_Int32 inputChromaFormat
XDAS_Int32 maxRules


Field Documentation

XDAS_Int32 IVIDANALYTICS_Params::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

XDAS_Int32 IVIDANALYTICS_Params::maxHeight

Maximum video height in pixels.

XDAS_Int32 IVIDANALYTICS_Params::maxWidth

Maximum video width in pixels.

XDAS_Int32 IVIDANALYTICS_Params::maxFrameRate

Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.

XDAS_Int32 IVIDANALYTICS_Params::dataEndianness

Endianness of output data.

See also:
XDM_DataFormat

XDAS_Int32 IVIDANALYTICS_Params::inputChromaFormat

Chroma format for the input buffer.

See also:
XDM_ChromaFormat

XDAS_Int32 IVIDANALYTICS_Params::maxRules

Maximum number of rules allowed.


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated