#include <iimgenc1.h>
size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxScans |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | forceChromaFormat |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Maximum height.
Maximum width.
Maximum number of scans.