#include <iimgenc1.h>
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numAU |
XDAS_Int32 | inputChromaFormat |
XDAS_Int32 | inputHeight |
XDAS_Int32 | inputWidth |
XDAS_Int32 | captureWidth |
XDAS_Int32 | generateHeader |
XDAS_Int32 | qValue |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Number of Access unit to encode. Set to XDM_DEFAULT to encode the entire frame.
Input frame height.
Input frame width.
Pitch. If set to zero, imageWidth is used; else, this field (assuming it's larger than imageWidth) is used.
Quality factor for encoder. Set to a value between 0 (lowest quality) and 100 (highest quality).