IAUDENC_InArgs Struct Reference
[XDM IAUDENC Audio Encoder Interface]

#include <iaudenc.h>


Detailed Description

Defines the input arguments for all IAUDENC instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.

The size field must be correctly set by the caller.

See also:
IAUDENC_Fxns::process()


Data Fields

XDAS_Int32 size


Field Documentation

XDAS_Int32 IAUDENC_InArgs::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated