#include <iaudenc1.h>
size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
XDAS_Int32 | bytesGenerated |
XDAS_Int32 | numZeroesPadded |
XDAS_Int32 | numInSamples |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.
Number of bytes generated during the process() call.
Number of zeroes padded to input.
Number of input samples per channel consumed by the encoder.