IAUDDEC_Params Struct Reference
[XDM IAUDDEC Audio Decoder Interface]

#include <iauddec.h>


Detailed Description

Defines the creation time parameters for all IAUDDEC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.

This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.

The size field must be correctly set by the caller.


Data Fields

XDAS_Int32 size
XDAS_Int32 maxSampleRate
XDAS_Int32 maxBitrate
XDAS_Int32 maxNoOfCh
XDAS_Int32 dataEndianness


Field Documentation

XDAS_Int32 IAUDDEC_Params::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

XDAS_Int32 IAUDDEC_Params::maxSampleRate

Maximum sampling frequency in Hz. For example, if the maximum sampling frequency is 44.1 kHz, this field should be 44100.

XDAS_Int32 IAUDDEC_Params::maxBitrate

Maximum bit rate in bits per second. For example, if the maximum bit rate is 128 kbps, set this field to 128000.

XDAS_Int32 IAUDDEC_Params::maxNoOfCh

Maximum Channels. See IAUDIO_ChannelId.

XDAS_Int32 IAUDDEC_Params::dataEndianness

Endianness of input data.

See also:
XDM_DataFormat


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated