#include <iauddec.h>
size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numBytes |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Size of valid input data (in bytes) to be processed.