Contiguous Memory Manager

Data Structures

struct  CMEM_AllocParams
 Parameters for CMEM_alloc(), CMEM_alloc2(), CMEM_allocPool(), CMEM_allocPool2(), CMEM_free(). More...
struct  CMEM_BlockAttrs

Defines

#define CMEM_VERSION   0x02200000U
#define CMEM_WB   0x0100
#define CMEM_INV   0x0200
#define CMEM_HEAP   0x0400
#define CMEM_POOL   0x0000
#define CMEM_CACHED   0x0800
#define CMEM_NONCACHED   0x0000
#define CMEM_PHYS   0x1000
#define CMEM_IOCALLOC   1
#define CMEM_IOCALLOCHEAP   2
#define CMEM_IOCFREE   3
#define CMEM_IOCGETPHYS   4
#define CMEM_IOCGETSIZE   5
#define CMEM_IOCGETPOOL   6
#define CMEM_IOCCACHE   7
#define CMEM_IOCGETVERSION   8
#define CMEM_IOCGETBLOCK   9
#define CMEM_IOCCACHEWBINV   CMEM_IOCCACHE | CMEM_WB | CMEM_INV
#define CMEM_IOCCACHEWB   CMEM_IOCCACHE | CMEM_WB
#define CMEM_IOCCACHEINV   CMEM_IOCCACHE | CMEM_INV
#define CMEM_IOCALLOCCACHED   CMEM_IOCALLOC | CMEM_CACHED
#define CMEM_IOCALLOCHEAPCACHED   CMEM_IOCALLOCHEAP | CMEM_CACHED
#define CMEM_IOCFREEHEAP   CMEM_IOCFREE | CMEM_HEAP
#define CMEM_IOCFREEPHYS   CMEM_IOCFREE | CMEM_PHYS
#define CMEM_IOCFREEHEAPPHYS   CMEM_IOCFREE | CMEM_HEAP | CMEM_PHYS
#define CMEM_IOCCMDMASK   0x000000ff

Functions

int CMEM_init (void)
 Initialize the CMEM module. Must be called before other API calls.
int CMEM_getPool (size_t size)
 Find the pool that best fits a given buffer size and has a buffer available.
int CMEM_getPool2 (int blockid, size_t size)
 Find the pool in memory block blockid that best fits a given buffer size and has a buffer available.
void * CMEM_allocPool (int poolid, CMEM_AllocParams *params)
 Allocate memory from a specified pool.
void * CMEM_allocPool2 (int blockid, int poolid, CMEM_AllocParams *params)
 Allocate memory from a specified pool in a specified memory block.
void * CMEM_alloc (size_t size, CMEM_AllocParams *params)
 Allocate memory of a specified size.
void * CMEM_alloc2 (int blockid, size_t size, CMEM_AllocParams *params)
 Allocate memory of a specified size from a specified memory block.
int CMEM_free (void *ptr, CMEM_AllocParams *params)
 Free a buffer previously allocated with CMEM_alloc()/ CMEM_allocPool().
unsigned long CMEM_getPhys (void *ptr)
 Get the physical address of a contiguous buffer.
int CMEM_cacheWb (void *ptr, size_t size)
 Do a cache writeback of the block pointed to by ptr/size.
int CMEM_cacheInv (void *ptr, size_t size)
 Do a cache invalidate of the block pointed to by ptr/size.
int CMEM_cacheWbInv (void *ptr, size_t size)
 Do a cache writeback/invalidate of the block pointed to by ptr/size.
int CMEM_getVersion (void)
 Retrieve version from CMEM driver.
int CMEM_getBlock (unsigned long *pphys_base, size_t *psize)
 Retrieve memory block bounds from CMEM driver.
int CMEM_getBlockAttrs (int blockid, CMEM_BlockAttrs *pattrs)
 Retrieve extended memory block attributes from CMEM driver.
int CMEM_exit (void)
 Finalize the CMEM module.

Variables

CMEM_AllocParams CMEM_DEFAULTPARAMS

Detailed Description

This is the API for the Contiguous Memory Manager.


Define Documentation

#define CMEM_VERSION   0x02200000U
#define CMEM_WB   0x0100
#define CMEM_INV   0x0200
#define CMEM_HEAP   0x0400

operation applies to heap

#define CMEM_POOL   0x0000

operation applies to a pool

#define CMEM_CACHED   0x0800

allocated buffer is cached

#define CMEM_NONCACHED   0x0000

allocated buffer is not cached

#define CMEM_PHYS   0x1000
#define CMEM_IOCALLOC   1
#define CMEM_IOCALLOCHEAP   2
#define CMEM_IOCFREE   3
#define CMEM_IOCGETPHYS   4
#define CMEM_IOCGETSIZE   5
#define CMEM_IOCGETPOOL   6
#define CMEM_IOCCACHE   7
#define CMEM_IOCGETVERSION   8
#define CMEM_IOCGETBLOCK   9
#define CMEM_IOCCACHEWBINV   CMEM_IOCCACHE | CMEM_WB | CMEM_INV
#define CMEM_IOCCACHEWB   CMEM_IOCCACHE | CMEM_WB
#define CMEM_IOCCACHEINV   CMEM_IOCCACHE | CMEM_INV
#define CMEM_IOCALLOCCACHED   CMEM_IOCALLOC | CMEM_CACHED
#define CMEM_IOCALLOCHEAPCACHED   CMEM_IOCALLOCHEAP | CMEM_CACHED
#define CMEM_IOCFREEHEAP   CMEM_IOCFREE | CMEM_HEAP
#define CMEM_IOCFREEPHYS   CMEM_IOCFREE | CMEM_PHYS
#define CMEM_IOCFREEHEAPPHYS   CMEM_IOCFREE | CMEM_HEAP | CMEM_PHYS
#define CMEM_IOCCMDMASK   0x000000ff

Function Documentation

int CMEM_init ( void   ) 

Initialize the CMEM module. Must be called before other API calls.

Returns:
0 for success or -1 for failure.
See also:
CMEM_exit
int CMEM_getPool ( size_t  size  ) 

Find the pool that best fits a given buffer size and has a buffer available.

Parameters:
size The buffer size for which a pool is needed.
Returns:
A poolid that can be passed to CMEM_allocPool(), or -1 for error.
Precondition:
Must have called CMEM_init()
See also:
CMEM_allocPool()
CMEM_allocPool2()
CMEM_free()
CMEM_getPool2()
int CMEM_getPool2 ( int  blockid,
size_t  size 
)

Find the pool in memory block blockid that best fits a given buffer size and has a buffer available.

Parameters:
blockid Block number
size The buffer size for which a pool is needed.
Returns:
A poolid that can be passed to CMEM_allocPool2(), or -1 for error.
Precondition:
Must have called CMEM_init()
See also:
CMEM_allocPool()
CMEM_allocPool2()
CMEM_free()
CMEM_getPool()
void* CMEM_allocPool ( int  poolid,
CMEM_AllocParams params 
)

Allocate memory from a specified pool.

Parameters:
poolid The pool from which to allocate memory.
params Allocation parameters.
Remarks:
params->type is ignored - a pool will always be used.
params->alignment is unused, since pool buffers are already aligned to specific boundaries.
Returns:
A pointer to the allocated buffer, or NULL for failure.
Precondition:
Must have called CMEM_init()
See also:
CMEM_alloc()
CMEM_alloc2()
CMEM_allocPool2()
CMEM_free()
void* CMEM_allocPool2 ( int  blockid,
int  poolid,
CMEM_AllocParams params 
)

Allocate memory from a specified pool in a specified memory block.

Parameters:
blockid The memory block from which to allocate.
poolid The pool from which to allocate memory.
params Allocation parameters.
Remarks:
params->type is ignored - a pool will always be used.
params->alignment is unused, since pool buffers are already aligned to specific boundaries.
Returns:
A pointer to the allocated buffer, or NULL for failure.
Precondition:
Must have called CMEM_init()
See also:
CMEM_alloc()
CMEM_alloc2()
CMEM_allocPool()
CMEM_free()
void* CMEM_alloc ( size_t  size,
CMEM_AllocParams params 
)

Allocate memory of a specified size.

Parameters:
size The size of the buffer to allocate.
params Allocation parameters.
Remarks:
Used to allocate memory from either a pool or the heap. If doing a pool allocation, the pool that best fits the requested size will be selected. Use CMEM_allocPool() to allocate from a specific pool. Allocation will be cached or noncached, as specified by params. params->alignment valid only for heap allocation.
Returns:
A pointer to the allocated buffer, or NULL for failure.
Precondition:
Must have called CMEM_init()
See also:
CMEM_allocPool()
CMEM_allocPool2()
CMEM_alloc2()
CMEM_free()
void* CMEM_alloc2 ( int  blockid,
size_t  size,
CMEM_AllocParams params 
)

Allocate memory of a specified size from a specified memory block.

Parameters:
blockid The memory block from which to allocate.
size The size of the buffer to allocate.
params Allocation parameters.
Remarks:
Used to allocate memory from either a pool or the heap. If doing a pool allocation, the pool that best fits the requested size will be selected. Use CMEM_allocPool() to allocate from a specific pool.
Allocation will be cached or noncached, as specified by params. params->alignment valid only for heap allocation.
Returns:
A pointer to the allocated buffer, or NULL for failure.
Precondition:
Must have called CMEM_init()
See also:
CMEM_allocPool()
CMEM_allocPool2()
CMEM_alloc()
CMEM_free()
int CMEM_free ( void *  ptr,
CMEM_AllocParams params 
)

Free a buffer previously allocated with CMEM_alloc()/ CMEM_allocPool().

Parameters:
ptr The pointer to the buffer.
params Allocation parameters.
Remarks:
Use the same CMEM_AllocParams as was used for the allocation. params->flags is "don't care". params->alignment is "don't care".
Returns:
0 for success or -1 for failure.
Precondition:
Must have called CMEM_init()
See also:
CMEM_alloc()
CMEM_alloc2()
CMEM_allocPool()
CMEM_allocPool2()
unsigned long CMEM_getPhys ( void *  ptr  ) 

Get the physical address of a contiguous buffer.

Parameters:
ptr The pointer to the buffer.
Returns:
The physical address of the buffer or 0 for failure.
Precondition:
Must have called CMEM_init()
int CMEM_cacheWb ( void *  ptr,
size_t  size 
)

Do a cache writeback of the block pointed to by ptr/size.

Parameters:
ptr Pointer to block to writeback
size Size in bytes of block to writeback.
Returns:
Success/failure boolean value
Precondition:
Must have called CMEM_init()
See also:
CMEM_cacheInv()
CMEM_cacheWbInv()
int CMEM_cacheInv ( void *  ptr,
size_t  size 
)

Do a cache invalidate of the block pointed to by ptr/size.

Parameters:
ptr Pointer to block to invalidate
size Size in bytes of block to invalidate
Returns:
Success/failure boolean value
Precondition:
Must have called CMEM_init()
See also:
CMEM_cacheWb()
CMEM_cacheWbInv()
int CMEM_cacheWbInv ( void *  ptr,
size_t  size 
)

Do a cache writeback/invalidate of the block pointed to by ptr/size.

Parameters:
ptr Pointer to block to writeback/invalidate
size Size in bytes of block to writeback/invalidate
Returns:
Success/failure boolean value
Precondition:
Must have called CMEM_init()
See also:
CMEM_cacheInv()
CMEM_cacheWb()
int CMEM_getVersion ( void   ) 

Retrieve version from CMEM driver.

Returns:
Installed CMEM driver's version number.
Precondition:
Must have called CMEM_init()
int CMEM_getBlock ( unsigned long *  pphys_base,
size_t *  psize 
)

Retrieve memory block bounds from CMEM driver.

Parameters:
pphys_base Pointer to storage for base physical address of CMEM's memory block
psize Pointer to storage for size of CMEM's memory block
Returns:
Success (0) or failure (-1).
Precondition:
Must have called CMEM_init()
See also:
CMEM_getBlockAttrs()
int CMEM_getBlockAttrs ( int  blockid,
CMEM_BlockAttrs pattrs 
)

Retrieve extended memory block attributes from CMEM driver.

Parameters:
blockid Block number
pattrs Pointer to CMEM_BlockAttrs struct
Returns:
Success (0) or failure (-1).
Remarks:
Currently this API returns the same values as CMEM_getBlock().
Precondition:
Must have called CMEM_init()
See also:
CMEM_getBlock()
int CMEM_exit ( void   ) 

Finalize the CMEM module.

Returns:
0 for success or -1 for failure.
Remarks:
After this function has been called, no other CMEM function may be called (unless CMEM is reinitialized).
Precondition:
Must have called CMEM_init()
See also:
CMEM_init()

Variable Documentation


Copyright 2010, Texas Instruments Incorporated