| module ti.uia.events.UIAProfile |
 |
 |
 |
UIA Profile Events
The UIAProfile module defines events that allow
tooling to analyze the performance of the software
(processing time, latency, etc.). These events are
designed to be logged from function-entry and function-exit
hook functions that are called by compiler-generated code
[
more ... ]
#include <ti/uia/events/UIAProfile.h>
Functions common to all target modules |
|
|
Constants |
| |
| |
| |
| |
DETAILS
The UIAProfile module defines events that allow
tooling to analyze the performance of the software
(processing time, latency, etc.). These events are
designed to be logged from function-entry and function-exit
hook functions that are called by compiler-generated code
TI compilers can be configured to either pass in a parameter
to the hook functions containing either the address
of the function or the name of the function.
If the compiler is configured to pass in the address of the function,
the UIAProfile_enterFunctionAdrs event should be logged by the
entry hook function and the UIAProfile_exitFunctionAdrs event
should be logged by the exit hook function.
If the compiler is configured to pass in the name of the function,
the UIAProfile_enterFunctionName event should be logged by the
entry hook function and the UIAProfile_exitFunctionName event
should be logged by the exit hook function.
When logging events using the xdc.runtime.Log module, the generation
of UIAProfile events is controlled by the Diags.ENTRY and Diags.EXIT
flags in a module's diagnostics mask. (For more information on
diagnostics masks, please see the xdc.runtime.Diags documentation.)
By default, the UIAProfile module will automatically set both the
Main.common$.Diags_ENTRY and Main.common$.Diags_EXIT flags to
Diags.ALWAYS_ON if these flags have not been previously configured.
To turn off these flags at configuration time, set
UIAProfile.enable = false; To allow these flags to be configured
at run time, set UIAProfile.runtimeControl = true;
EXAMPLES
Example 1: This is part of the XDC configuration file for the application:
var UIAProfile = xdc.useModule('ti.uia.events.UIAProfile');
var LoggingSetup = xdc.useModule('ti.uia.sysbios.LoggingSetup');
Example 2: The following example configures a module to support logging
of ENTRY and EXIT events, but defers the actual activation and deactivation of the
logging until runtime. See the
Diags_setMask()
function for details on specifying the control string.
This is a part of the XDC configuration file for the application:
var UIAProfile = xdc.useModule('ti.uia.events.UIAProfile');
UIAProfile.runtimeControl = true;
UIAProfile.enable = false;
This is a part of the C code for the application.
The diags_ENTRY mask is set by "E", and the diags_EXIT mask is set by "X".
#include <xdc/runtime/Diags.h>
#include <xdc/runtime/Main.h>
// turn on logging of ENTRY and EXIT events in the module
Diags_setMask("xdc.runtime.Main+EX");
// turn off logging of ENTRY and EXIT events in the module
Diags_setMask("xdc.runtime.Main-EX");
| config UIAProfile_enterFunctionAdrs // module-wide |
 |
Profiling event used to log the entry point of a function
extern const Log_Event UIAProfile_enterFunctionAdrs;
VALUES
taskHandle
task handle that identifies the currently active task (use 0 if not required)
functionAdrs
the address of a function that can differentiate this pair of start and stop events from others
EXAMPLE
To add entry and exit hook functions to every function
1. Use the following compiler options when compiling the source
--entry_hook=functionEntryHook
--entry_param=address
--exit_hook=functionExitHook
--exit_param=address
2. Add the following c code to implement the hook functions:
The first parameter (the taskHandle) is set to 0 in this example.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAProfile.h>
...
void functionEntryHook(void (*adrs)()){
Log_write2(UIAProfile_enterFunctionAdrs, 0,(IArg)adrs);
...
void functionExitHook( void (*adrs)() ){
Log_write2(UIAProfile_exitFunctionAdrs, 0,(IArg)adrs);
}
The following text will be displayed for the event:
enterFunctionAdrs: taskHandle=0x0, adrs=0x820060
exitFunctionAdrs: taskHandle0x0, adrs=0x820060
SEE
| config UIAProfile_enterFunctionName // module-wide |
 |
Profiling event used to log the entry point of a function
extern const Log_Event UIAProfile_enterFunctionName;
VALUES
taskHandle
task handle that identifies the currently active task (use 0 if not required)
functionName
the (const char*) name of the function that is passed to the hook fn by the compiler
EXAMPLE
To add entry and exit hook functions to every function
1. Use the following compiler options when compiling the source
--entry_hook=functionEntryHook
--entry_param=name
--exit_hook=functionExitHook
--exit_param=name
2. Add the following c code to implement the hook functions:
The first parameter (the taskHandle) is set to 0 in this example.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAProfile.h>
...
void functionEntryHook(const char* name){
Log_write2(UIAProfile_enterFunctionName, 0,(IArg)name);
...
void functionExitHook(const char* name){
Log_write2(UIAProfile_exitFunctionName, 0,(IArg)name);
}
The following text will be displayed for the event:
enterFunctionName: taskHandle=0x0, name=myFunctionName
exitFunctionName: taskHandle0x0, name=myFunctionName
SEE
| config UIAProfile_exitFunctionAdrs // module-wide |
 |
Profiling event used to log the exit point of a function
extern const Log_Event UIAProfile_exitFunctionAdrs;
VALUES
taskHandle
task handle that identifies the currently active task (use 0 if not required)
functionAdrs
the address of a function that can differentiate this pair of start and stop events from others
EXAMPLE
To add entry and exit hook functions to every function
1. Use the following compiler options when compiling the source
--entry_hook=functionEntryHook
--entry_param=address
--exit_hook=functionExitHook
--exit_param=address
2. Add the following c code to implement the hook functions:
Task_selfMacro() is used to get the current task handle in this example.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAProfile.h>
#include <ti/sysbios/knl/Task.h>
...
void functionEntryHook(void (*adrs)()){
Log_write2(UIAProfile_enterFunctionAdrs, (IArg)Task_selfMacro(),(IArg)addr);
...
void functionExitHook( void (*adrs)() ){
Log_write2(UIAProfile_exitFunctionAdrs, (IArg)Task_selfMacro(),(IArg)addr);
}
The following text will be displayed for the event:
enterFunctionAdrs: taskHandle=0x0, adrs=0x820060
exitFunctionAdrs: taskHandle=0x0, adrs=0x820060
SEE
| config UIAProfile_exitFunctionName // module-wide |
 |
Profiling event used to log the exit point of a function
extern const Log_Event UIAProfile_exitFunctionName;
VALUES
taskHandle
task handle that identifies the currently active task (use 0 if not required)
functionName
the (const char*) name of the function that is passed to the hook fn by the compiler
EXAMPLE
To add entry and exit hook functions to every function
1. Use the following compiler options when compiling the source
--entry_hook=functionEntryHook
--entry_param=name
--exit_hook=functionExitHook
--exit_param=name
2. Add the following c code to implement the hook functions:
Task_selfMacro() is used to get the current task handle in this example.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAProfile.h>
#include <ti/sysbios/knl/Task.h>
...
void functionEntryHook(const char* name){
Log_write2(UIAProfile_enterFunctionName, (IArg)Task_selfMacro(),(IArg)name);
...
void functionExitHook(const char* name){
Log_write2(UIAProfile_exitFunctionName, (IArg)Task_selfMacro(),(IArg)name);
}
The following text will be displayed for the event:
enterFunctionName: taskHandle=0x0, adrs=myFunctionName
exitFunctionName: taskHandle=0x0, name=myFunctionName
SEE
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool UIAProfile_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool UIAProfile_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 UIAProfile_Module_getMask();
// Returns the diagnostics mask for this module
Void UIAProfile_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var UIAProfile = xdc.useModule('ti.uia.events.UIAProfile');
module-wide config parameters
msg: "enterFunctionAdrs: taskHandle=0x%x, adrs=0x%x"
};
msg: "enterFunctionName: taskHandle=0x%x, name=%s"
};
msg: "exitFunctionAdrs: taskHandle=0x%x, adrs=0x%x"
};
msg: "exitFunctionName: taskHandle=0x%x, name=%s"
};
| config UIAProfile.enterFunctionAdrs // module-wide |
 |
Profiling event used to log the entry point of a function
msg: "enterFunctionAdrs: taskHandle=0x%x, adrs=0x%x"
};
VALUES
taskHandle
task handle that identifies the currently active task (use 0 if not required)
functionAdrs
the address of a function that can differentiate this pair of start and stop events from others
EXAMPLE
To add entry and exit hook functions to every function
1. Use the following compiler options when compiling the source
--entry_hook=functionEntryHook
--entry_param=address
--exit_hook=functionExitHook
--exit_param=address
2. Add the following c code to implement the hook functions:
The first parameter (the taskHandle) is set to 0 in this example.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAProfile.h>
...
void functionEntryHook(void (*adrs)()){
Log_write2(UIAProfile_enterFunctionAdrs, 0,(IArg)adrs);
...
void functionExitHook( void (*adrs)() ){
Log_write2(UIAProfile_exitFunctionAdrs, 0,(IArg)adrs);
}
The following text will be displayed for the event:
enterFunctionAdrs: taskHandle=0x0, adrs=0x820060
exitFunctionAdrs: taskHandle0x0, adrs=0x820060
SEE
C SYNOPSIS
| config UIAProfile.enterFunctionName // module-wide |
 |
Profiling event used to log the entry point of a function
msg: "enterFunctionName: taskHandle=0x%x, name=%s"
};
VALUES
taskHandle
task handle that identifies the currently active task (use 0 if not required)
functionName
the (const char*) name of the function that is passed to the hook fn by the compiler
EXAMPLE
To add entry and exit hook functions to every function
1. Use the following compiler options when compiling the source
--entry_hook=functionEntryHook
--entry_param=name
--exit_hook=functionExitHook
--exit_param=name
2. Add the following c code to implement the hook functions:
The first parameter (the taskHandle) is set to 0 in this example.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAProfile.h>
...
void functionEntryHook(const char* name){
Log_write2(UIAProfile_enterFunctionName, 0,(IArg)name);
...
void functionExitHook(const char* name){
Log_write2(UIAProfile_exitFunctionName, 0,(IArg)name);
}
The following text will be displayed for the event:
enterFunctionName: taskHandle=0x0, name=myFunctionName
exitFunctionName: taskHandle0x0, name=myFunctionName
SEE
C SYNOPSIS
| config UIAProfile.exitFunctionAdrs // module-wide |
 |
Profiling event used to log the exit point of a function
msg: "exitFunctionAdrs: taskHandle=0x%x, adrs=0x%x"
};
VALUES
taskHandle
task handle that identifies the currently active task (use 0 if not required)
functionAdrs
the address of a function that can differentiate this pair of start and stop events from others
EXAMPLE
To add entry and exit hook functions to every function
1. Use the following compiler options when compiling the source
--entry_hook=functionEntryHook
--entry_param=address
--exit_hook=functionExitHook
--exit_param=address
2. Add the following c code to implement the hook functions:
Task_selfMacro() is used to get the current task handle in this example.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAProfile.h>
#include <ti/sysbios/knl/Task.h>
...
void functionEntryHook(void (*adrs)()){
Log_write2(UIAProfile_enterFunctionAdrs, (IArg)Task_selfMacro(),(IArg)addr);
...
void functionExitHook( void (*adrs)() ){
Log_write2(UIAProfile_exitFunctionAdrs, (IArg)Task_selfMacro(),(IArg)addr);
}
The following text will be displayed for the event:
enterFunctionAdrs: taskHandle=0x0, adrs=0x820060
exitFunctionAdrs: taskHandle=0x0, adrs=0x820060
SEE
C SYNOPSIS
| config UIAProfile.exitFunctionName // module-wide |
 |
Profiling event used to log the exit point of a function
msg: "exitFunctionName: taskHandle=0x%x, name=%s"
};
VALUES
taskHandle
task handle that identifies the currently active task (use 0 if not required)
functionName
the (const char*) name of the function that is passed to the hook fn by the compiler
EXAMPLE
To add entry and exit hook functions to every function
1. Use the following compiler options when compiling the source
--entry_hook=functionEntryHook
--entry_param=name
--exit_hook=functionExitHook
--exit_param=name
2. Add the following c code to implement the hook functions:
Task_selfMacro() is used to get the current task handle in this example.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAProfile.h>
#include <ti/sysbios/knl/Task.h>
...
void functionEntryHook(const char* name){
Log_write2(UIAProfile_enterFunctionName, (IArg)Task_selfMacro(),(IArg)name);
...
void functionExitHook(const char* name){
Log_write2(UIAProfile_exitFunctionName, (IArg)Task_selfMacro(),(IArg)name);
}
The following text will be displayed for the event:
enterFunctionName: taskHandle=0x0, adrs=myFunctionName
exitFunctionName: taskHandle=0x0, name=myFunctionName
SEE
C SYNOPSIS
| metaonly config UIAProfile.common$ // module-wide |
 |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
| metaonly config UIAProfile.enable // module-wide |
 |
Specify whether profile events are enabled or disabled
(set to true by default)
UIAProfile.enable = Bool true;
DETAILS
if the UIAProfile enable config property is true (default):
If runtimeControl = 'false' the diags bits will be configured as
ALWAYS_ON, meaning they can't be changed at runtime.
If runtimeControl = 'true', the bits will be configured as 'RUNTIME_ON'.
if the UIAProfile enable config property is false:
If runtimeControl = 'false' the diags bits will be configured as
ALWAYS_OFF, meaning they can't be changed at runtime.
If runtimeControl = 'true', the bits will be configured as 'RUNTIME_OFF'.
| metaonly config UIAProfile.isContextAwareProfilingEnabled // module-wide |
 |
Specify whether the task context that the function is executing within is logged or not
Set to false if not using Sys/BIOS or to reduce CPU overhead
UIAProfile.isContextAwareProfilingEnabled = Bool true;
| metaonly config UIAProfile.runtimeControl // module-wide |
 |
Specify whether profile events can be enabled / disabled at runtime.
(set to false by default)
UIAProfile.runtimeControl = Bool false;
DETAILS
This determines what diags settings are applied to the module's diags
mask.
if the UIAProfile enable config property is true (default):
If runtimeControl = 'false' the diags bits will be configured as
ALWAYS_ON, meaning they can't be changed at runtime.
If runtimeControl = 'true', the bits will be configured as 'RUNTIME_ON'.
if the UIAProfile enable config property is false:
If runtimeControl = 'false' the diags bits will be configured as
ALWAYS_OFF, meaning they can't be changed at runtime.
If runtimeControl = 'true', the bits will be configured as 'RUNTIME_OFF'.
generated on Tue, 14 Feb 2017 00:15:09 GMT