TI-RTOS Drivers
tidrivers_full_2_20_00_08
|
Macros | |
#define | UART_STATUS_SUCCESS 0 |
Successful status code returned by UART_control(). More... | |
#define | UART_STATUS_ERROR -1 |
Generic error status code returned by UART_control(). More... | |
#define | UART_STATUS_UNDEFINEDCMD -2 |
An error status code returned by UART_control() for undefined command codes. More... | |
UART_STATUS_* macros are general status codes returned by UART_control()
UARTCC26XX_STATUS_* macros are command codes only defined in the UARTCC26XX.h driver implementation and need to:
UARTCC3200_STATUS_* macros are command codes only defined in the UARTCC3200.h driver implementation and need to:
UARTCC3200DMA_STATUS_* macros are command codes only defined in the UARTCC3200DMA.h driver implementation and need to:
UARTEUSCIA_STATUS_* macros are command codes only defined in the UARTEUSCIA.h driver implementation and need to:
UARTMSP432_STATUS_* macros are command codes only defined in the UARTMSP432.h driver implementation and need to:
UARTTivaDMA_STATUS_* macros are command codes only defined in the UARTTivaDMA.h driver implementation and need to:
UARTUSCIA_STATUS_* macros are command codes only defined in the UARTUSCIA.h driver implementation and need to:
#define UART_STATUS_SUCCESS 0 |
Successful status code returned by UART_control().
UART_control() returns UART_STATUS_SUCCESS if the control code was executed successfully.
#define UART_STATUS_ERROR -1 |
Generic error status code returned by UART_control().
UART_control() returns UART_STATUS_ERROR if the control code was not executed successfully.
#define UART_STATUS_UNDEFINEDCMD -2 |
An error status code returned by UART_control() for undefined command codes.
UART_control() returns UART_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.