49 #ifndef ti_drivers_uart_UARTCC3200DMA__include
50 #define ti_drivers_uart_UARTCC3200DMA__include
UART_STOP
UART stop bit settings.
Definition: UART.h:410
unsigned int readTimeout
Definition: UARTCC3200DMA.h:160
uDMA driver implementation for CC3200.
UART_Echo readEcho
Definition: UARTCC3200DMA.h:171
Clock interface for the RTOS Porting Interface.
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:528
UART_PAR
UART parity type settings.
Definition: UART.h:420
UART_DataMode writeDataMode
Definition: UARTCC3200DMA.h:166
struct UARTCC3200DMA_Object UARTCC3200DMA_Object
UARTCC3200DMA Object.
UART_Mode
UART mode settings.
Definition: UART.h:322
UDMACC3200_Handle dmaHandle
Definition: UARTCC3200DMA.h:195
UART_DataMode
UART data mode settings.
Definition: UART.h:370
struct UARTCC3200DMA_HWAttrs UARTCC3200DMA_HWAttrs
UARTCC3200DMA Hardware attributes.
UART_ReturnMode
UART return mode settings.
Definition: UART.h:355
Power_NotifyObj postNotify
Definition: UARTCC3200DMA.h:191
size_t readCount
Definition: UARTCC3200DMA.h:180
UART_Echo
UART echo settings.
Definition: UART.h:388
uint32_t baudRate
Definition: UARTCC3200DMA.h:167
void * SemaphoreP_Handle
Opaque client reference to an instance of a SemaphoreP.
Definition: SemaphoreP.h:96
Semaphore module for the RTOS Porting Interface.
UART_DataMode readDataMode
Definition: UARTCC3200DMA.h:165
ClockP_Handle txFifoEmptyClk
Definition: UARTCC3200DMA.h:190
SemaphoreP_Handle readSem
Definition: UARTCC3200DMA.h:185
size_t writeSize
Definition: UARTCC3200DMA.h:176
void * readBuf
Definition: UARTCC3200DMA.h:179
UART_Mode readMode
Definition: UARTCC3200DMA.h:158
unsigned int intNum
Definition: UARTCC3200DMA.h:141
Power notify object structure.
Definition: Power.h:112
UART_STOP stopBits
Definition: UARTCC3200DMA.h:169
SemaphoreP_Handle writeSem
Definition: UARTCC3200DMA.h:184
UDMACC3200 Global configuration.
Definition: UDMACC3200.h:135
UART_LEN dataLength
Definition: UARTCC3200DMA.h:168
unsigned int intPriority
Definition: UARTCC3200DMA.h:143
const UART_FxnTable UARTCC3200DMA_fxnTable
const void * writeBuf
Definition: UARTCC3200DMA.h:174
void(* UART_Callback)(UART_Handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:315
UART_PAR parityType
Definition: UARTCC3200DMA.h:170
UARTCC3200DMA Hardware attributes.
Definition: UARTCC3200DMA.h:137
unsigned long rxChannelIndex
Definition: UARTCC3200DMA.h:145
unsigned int writeTimeout
Definition: UARTCC3200DMA.h:161
HwiP_Handle hwiHandle
Definition: UARTCC3200DMA.h:187
unsigned int baseAddr
Definition: UARTCC3200DMA.h:139
size_t readSize
Definition: UARTCC3200DMA.h:181
UART_LEN
UART data length settings.
Definition: UART.h:398
UART_Callback writeCallback
Definition: UARTCC3200DMA.h:163
size_t writeCount
Definition: UARTCC3200DMA.h:175
unsigned int powerMgrId
Definition: UARTCC3200DMA.h:192
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:66
UART_ReturnMode readReturnMode
Definition: UARTCC3200DMA.h:164
UARTCC3200DMA Object.
Definition: UARTCC3200DMA.h:155
struct UARTCC3200DMA_Object * UARTCC3200DMA_Handle
UART_Callback readCallback
Definition: UARTCC3200DMA.h:162
unsigned long txChannelIndex
Definition: UARTCC3200DMA.h:147
Hardware Interrupt module for the RTOS Porting Interface.
bool opened
Definition: UARTCC3200DMA.h:157
UART_Mode writeMode
Definition: UARTCC3200DMA.h:159
void * ClockP_Handle
Opaque client reference to an instance of a ClockP.
Definition: ClockP.h:91