TI-RTOS Drivers  tidrivers_msp43x_2_16_01_13
Data Structures | Macros | Typedefs | Enumerations | Functions
SPI.h File Reference

Detailed Description

SPI driver interface.

============================================================================

The SPI header file should be included in an application as follows:

#include <ti/drivers/SPI.h>

Operation

The SPI driver in TI-RTOS is designed to serve a means to move data between SPI peripherals. This driver does not interpret any of the data sent to or received from this peripheral.

The APIs in this driver serve as an interface to a typical TI-RTOS application. The specific peripheral implementations are responsible to create all the SYS/BIOS specific primitives to allow for thread-safe operation.

The SPI driver operates on some key definitions and assumptions:

Opening the driver

SPI_Handle handle;
SPI_Params params;
SPI_Transaction spiTransaction;
SPI_Params_init(&params);
params.bitRate = someNewBitRate;
handle = SPI_open(someSPI_configIndexValue, &params);
if (!handle) {
System_printf("SPI did not open");
}

Transferring data

Data transmitted and received by the SPI peripheral is performed using SPI_transfer(). SPI_transfer() accepts a pointer to a SPI_Transaction structure that dictates what quantity of data is sent and received.

SPI_Transaction spiTransaction;
spiTransaction.count = someIntegerValue;
spiTransaction.txBuf = transmitBufferPointer;
spiTransaction.rxBuf = receiveBufferPointer;
ret = SPI_transfer(handle, &spiTransaction);
if (!ret) {
System_printf("Unsuccessful SPI transfer");
}

Canceling a transaction

SPI_transferCancel() is used to cancel a SPI transaction when the driver is used in SPI_MODE_CALLBACK mode.

Calling this API while no transfer is in progress has no effect. If a transfer is in progress, it canceled and a callback on the SPI_CallbackFxn is performed. The SPI_Status status field in the SPI_Transaction struct can be examined within the callback to determine if the transaction was successful.

Implementation

This module serves as the main interface for TI-RTOS applications. Its purpose is to redirect the module's APIs to specific peripheral implementations which are specified using a pointer to a SPI_FxnTable.

The SPI driver interface module is joined (at link time) to a NULL-terminated array of SPI_Config data structures named SPI_config. SPI_config is implemented in the application with each entry being an instance of a SPI peripheral. Each entry in SPI_config contains a:

Instrumentation

The SPI driver interface produces log statements if instrumentation is enabled.

Diagnostics Mask Log details
Diags_USER1 basic operations performed
Diags_USER2 detailed operations performed

#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
Include dependency graph for SPI.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  SPI_Transaction
 A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK. More...
 
struct  SPI_Params
 SPI Parameters. More...
 
struct  SPI_FxnTable
 The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation. More...
 
struct  SPI_Config
 SPI Global configuration. More...
 

Macros

#define SPI_CMD_RESERVED   32
 
#define SPI_STATUS_RESERVED   -32
 
#define SPI_STATUS_SUCCESS   0
 Successful status code returned by SPI_control(). More...
 
#define SPI_STATUS_ERROR   -1
 Generic error status code returned by SPI_control(). More...
 
#define SPI_STATUS_UNDEFINEDCMD   -2
 An error status code returned by SPI_control() for undefined command codes. More...
 
#define SPI_WAIT_FOREVER   ~(0)
 Wait forever define. More...
 

Typedefs

typedef struct SPI_ConfigSPI_Handle
 A handle that is returned from a SPI_open() call. More...
 
typedef enum SPI_Status SPI_Status
 Status codes that are set by the SPI driver. More...
 
typedef struct SPI_Transaction SPI_Transaction
 A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK. More...
 
typedef void(* SPI_CallbackFxn) (SPI_Handle handle, SPI_Transaction *transaction)
 The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK. More...
 
typedef enum SPI_Mode SPI_Mode
 Definitions for various SPI modes of operation. More...
 
typedef enum SPI_FrameFormat SPI_FrameFormat
 Definitions for various SPI data frame formats. More...
 
typedef enum SPI_TransferMode SPI_TransferMode
 SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously. In SPI_MODE_BLOCKING mode SPI_transfer() blocks code execution until the SPI transaction has completed. In SPI_MODE_CALLBACK SPI_transfer() does not block code execution and instead calls a SPI_CallbackFxn callback function when the transaction has completed. More...
 
typedef struct SPI_Params SPI_Params
 SPI Parameters. More...
 
typedef void(* SPI_CloseFxn) (SPI_Handle handle)
 A function pointer to a driver specific implementation of SPI_close(). More...
 
typedef int(* SPI_ControlFxn) (SPI_Handle handle, unsigned int cmd, void *arg)
 A function pointer to a driver specific implementation of SPI_control(). More...
 
typedef void(* SPI_InitFxn) (SPI_Handle handle)
 A function pointer to a driver specific implementation of SPI_init(). More...
 
typedef SPI_Handle(* SPI_OpenFxn) (SPI_Handle handle, SPI_Params *params)
 A function pointer to a driver specific implementation of SPI_open(). More...
 
typedef void(* SPI_ServiceISRFxn) (SPI_Handle handle)
 A function pointer to a driver specific implementation of SPI_serviceISR(). More...
 
typedef bool(* SPI_TransferFxn) (SPI_Handle handle, SPI_Transaction *transaction)
 A function pointer to a driver specific implementation of SPI_transfer(). More...
 
typedef void(* SPI_TransferCancelFxn) (SPI_Handle handle)
 A function pointer to a driver specific implementation of SPI_transferCancel(). More...
 
typedef struct SPI_FxnTable SPI_FxnTable
 The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation. More...
 
typedef struct SPI_Config SPI_Config
 SPI Global configuration. More...
 

Enumerations

enum  SPI_Status {
  SPI_TRANSFER_COMPLETED = 0,
  SPI_TRANSFER_STARTED,
  SPI_TRANSFER_CANCELED,
  SPI_TRANSFER_FAILED,
  SPI_TRANSFER_CSN_DEASSERT
}
 Status codes that are set by the SPI driver. More...
 
enum  SPI_Mode {
  SPI_MASTER = 0,
  SPI_SLAVE = 1
}
 Definitions for various SPI modes of operation. More...
 
enum  SPI_FrameFormat {
  SPI_POL0_PHA0 = 0,
  SPI_POL0_PHA1 = 1,
  SPI_POL1_PHA0 = 2,
  SPI_POL1_PHA1 = 3,
  SPI_TI = 4,
  SPI_MW = 5
}
 Definitions for various SPI data frame formats. More...
 
enum  SPI_TransferMode {
  SPI_MODE_BLOCKING,
  SPI_MODE_CALLBACK
}
 SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously. In SPI_MODE_BLOCKING mode SPI_transfer() blocks code execution until the SPI transaction has completed. In SPI_MODE_CALLBACK SPI_transfer() does not block code execution and instead calls a SPI_CallbackFxn callback function when the transaction has completed. More...
 

Functions

void SPI_close (SPI_Handle handle)
 Function to close a SPI peripheral specified by the SPI handle. More...
 
int SPI_control (SPI_Handle handle, unsigned int cmd, void *arg)
 Function performs implementation specific features on a given SPI_Handle. More...
 
void SPI_init (void)
 This function initializes the SPI module. More...
 
SPI_Handle SPI_open (unsigned int index, SPI_Params *params)
 This function opens a given SPI peripheral. More...
 
void SPI_Params_init (SPI_Params *params)
 Function to initialize the SPI_Params struct to its defaults. More...
 
void SPI_serviceISR (SPI_Handle handle)
 Function to service the SPI module's interrupt service routine. More...
 
bool SPI_transfer (SPI_Handle handle, SPI_Transaction *transaction)
 Function to perform SPI transactions. More...
 
void SPI_transferCancel (SPI_Handle handle)
 Function to cancel SPI transactions. More...
 

Macro Definition Documentation

#define SPI_WAIT_FOREVER   ~(0)

Wait forever define.

Typedef Documentation

typedef struct SPI_Config* SPI_Handle

A handle that is returned from a SPI_open() call.

typedef enum SPI_Status SPI_Status

Status codes that are set by the SPI driver.

A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK.

typedef void(* SPI_CallbackFxn) (SPI_Handle handle, SPI_Transaction *transaction)

The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.

Parameters
SPI_HandleSPI_Handle
SPI_Transaction*SPI_Transaction*
typedef enum SPI_Mode SPI_Mode

Definitions for various SPI modes of operation.

Definitions for various SPI data frame formats.

SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously. In SPI_MODE_BLOCKING mode SPI_transfer() blocks code execution until the SPI transaction has completed. In SPI_MODE_CALLBACK SPI_transfer() does not block code execution and instead calls a SPI_CallbackFxn callback function when the transaction has completed.

typedef struct SPI_Params SPI_Params

SPI Parameters.

SPI Parameters are used to with the SPI_open() call. Default values for these parameters are set using SPI_Params_init().

See also
SPI_Params_init()
typedef void(* SPI_CloseFxn) (SPI_Handle handle)

A function pointer to a driver specific implementation of SPI_close().

typedef int(* SPI_ControlFxn) (SPI_Handle handle, unsigned int cmd, void *arg)

A function pointer to a driver specific implementation of SPI_control().

typedef void(* SPI_InitFxn) (SPI_Handle handle)

A function pointer to a driver specific implementation of SPI_init().

typedef SPI_Handle(* SPI_OpenFxn) (SPI_Handle handle, SPI_Params *params)

A function pointer to a driver specific implementation of SPI_open().

typedef void(* SPI_ServiceISRFxn) (SPI_Handle handle)

A function pointer to a driver specific implementation of SPI_serviceISR().

typedef bool(* SPI_TransferFxn) (SPI_Handle handle, SPI_Transaction *transaction)

A function pointer to a driver specific implementation of SPI_transfer().

typedef void(* SPI_TransferCancelFxn) (SPI_Handle handle)

A function pointer to a driver specific implementation of SPI_transferCancel().

typedef struct SPI_FxnTable SPI_FxnTable

The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation.

typedef struct SPI_Config SPI_Config

SPI Global configuration.

The SPI_Config structure contains a set of pointers used to characterize the SPI driver implementation.

This structure needs to be defined before calling SPI_init() and it must not be changed thereafter.

See also
SPI_init()

Enumeration Type Documentation

enum SPI_Status

Status codes that are set by the SPI driver.

Enumerator
SPI_TRANSFER_COMPLETED 
SPI_TRANSFER_STARTED 
SPI_TRANSFER_CANCELED 
SPI_TRANSFER_FAILED 
SPI_TRANSFER_CSN_DEASSERT 
enum SPI_Mode

Definitions for various SPI modes of operation.

Enumerator
SPI_MASTER 

SPI in master mode

SPI_SLAVE 

SPI in slave mode

Definitions for various SPI data frame formats.

Enumerator
SPI_POL0_PHA0 

SPI mode Polarity 0 Phase 0

SPI_POL0_PHA1 

SPI mode Polarity 0 Phase 1

SPI_POL1_PHA0 

SPI mode Polarity 1 Phase 0

SPI_POL1_PHA1 

SPI mode Polarity 1 Phase 1

SPI_TI 

TI mode

SPI_MW 

Micro-wire mode

SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously. In SPI_MODE_BLOCKING mode SPI_transfer() blocks code execution until the SPI transaction has completed. In SPI_MODE_CALLBACK SPI_transfer() does not block code execution and instead calls a SPI_CallbackFxn callback function when the transaction has completed.

Enumerator
SPI_MODE_BLOCKING 

SPI_transfer() blocks execution. This mode can only be used when called within a Task context

SPI_MODE_CALLBACK 

SPI_transfer() does not block code execution and will call a SPI_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context.

Function Documentation

void SPI_close ( SPI_Handle  handle)

Function to close a SPI peripheral specified by the SPI handle.

Precondition
SPI_open() has to be called first.
Parameters
handleA SPI handle returned from SPI_open()
See also
SPI_open()
int SPI_control ( SPI_Handle  handle,
unsigned int  cmd,
void *  arg 
)

Function performs implementation specific features on a given SPI_Handle.

Commands for SPI_control can originate from SPI.h or from implementation specific SPI*.h (SPICC26XX.h, SPITiva.h, etc.. ) files. While commands from SPI.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific SPI*.h files add unique driver capabilities but are not API portable across all SPI driver implementations.

Commands supported by SPI.h follow a SPI_CMD_<cmd> naming convention.
Commands supported by SPI*.h follow a SPI*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.

See SPI_control command codes for command codes.

See SPI_control return status codes for status codes.

Precondition
SPI_open() has to be called first.
Parameters
handleA SPI handle returned from SPI_open()
cmdSPI.h or SPI*.h commands.
argAn optional R/W (read/write) command argument accompanied with cmd
Returns
Implementation specific return codes. Negative values indicate unsuccessful operations.
See also
SPI_open()
void SPI_init ( void  )

This function initializes the SPI module.

Precondition
The SPI_config structure must exist and be persistent before this function can be called. This function must also be called before any other SPI driver APIs. This function call does not modify any peripheral registers.
SPI_Handle SPI_open ( unsigned int  index,
SPI_Params params 
)

This function opens a given SPI peripheral.

Precondition
SPI controller has been initialized using SPI_init()
Parameters
indexLogical peripheral number for the SPI indexed into the SPI_config table
paramsPointer to an parameter block, if NULL it will use default values. All the fields in this structure are RO (read-only).
Returns
A SPI_Handle on success or a NULL on an error or if it has been opened already.
See also
SPI_init()
SPI_close()
void SPI_Params_init ( SPI_Params params)

Function to initialize the SPI_Params struct to its defaults.

Parameters
paramsAn pointer to SPI_Params structure for initialization

Defaults values are: transferMode = SPI_MODE_BLOCKING transferTimeout = SPI_WAIT_FOREVER transferCallbackFxn = NULL mode = SPI_MASTER bitRate = 1000000 (Hz) dataSize = 8 (bits) frameFormat = SPI_POL0_PHA0

void SPI_serviceISR ( SPI_Handle  handle)

Function to service the SPI module's interrupt service routine.

This function is not supported on all driver implementations. Refer to implementation specific documentation for details.

Parameters
handleA SPI_Handle
bool SPI_transfer ( SPI_Handle  handle,
SPI_Transaction transaction 
)

Function to perform SPI transactions.

If the SPI is in SPI_MASTER mode, it will immediately start the transaction. If the SPI is in SPI_SLAVE mode, it prepares itself for a transaction with a SPI master.

In SPI_MODE_BLOCKING, SPI_transfer will block task execution until the transaction has completed.

In SPI_MODE_CALLBACK, SPI_transfer() does not block task execution and calls a SPI_CallbackFxn. This makes the SPI_tranfer() safe to be used within a Task, Swi, or Hwi context. The SPI_Transaction structure must stay persistent until the SPI_transfer function has completed!

Parameters
handleA SPI_Handle
transactionA pointer to a SPI_Transaction. All of the fields within transaction except SPI_Transaction.count and SPI_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occured, SPI_Transaction.count will contain the number of frames that were transferred.
Returns
true if started successfully; else false
See also
SPI_open
SPI_transferCancel
void SPI_transferCancel ( SPI_Handle  handle)

Function to cancel SPI transactions.

In SPI_MODE_BLOCKING, SPI_transferCancel has no effect.

In SPI_MODE_CALLBACK, SPI_transferCancel() will stop an SPI transfer if if one is in progress. If a transaction was in progress, its callback function will be called in context from which this API is called from. The SPI_CallbackFxn function can determine if the transaction was successful or not by reading the SPI_Status status value in the SPI_Transaction structure.

Parameters
handleA SPI_Handle
See also
SPI_open
SPI_transfer
Copyright 2016, Texas Instruments Incorporated