TI-Drivers is a software component that includes device drivers for the assorted peripherals on a given device (i.e., UART, SPI, I2C, etc.).
These device drivers are also included in the TI-RTOS product. They are provided here as a separate component so that they can be used as a stand-alone library in non-TI-RTOS environments. To avoid duplication, TI-RTOS includes this versioned component in the tirtos/products directory.
The following documentation is provided with this release.
License and manifest.
Release notes from previous releases are also available in the release notes archive directory.
Key | Summary |
---|---|
TIDRIVERS-155 | Need to add cdoc to TIDrivers release notes |
TIDRIVERS-153 | Improve SYSTICK sync to RTC if device wakes late from LPDS |
TIDRIVERS-152 | CC3200 device may fail to wake from Low Power Deep Sleep (LPDS) |
TIDRIVERS-151 | The tidrivers component needs cdoc |
TIDRIVERS-149 | Ship PDM *.c sources and update the licenses for the codec and asm files| |TIDRIVERS-144|Enable user-provided SimpleLink libraries| |TIDRIVERS-87|Power_init() must support being called multiple times| |TIDRIVERS-73|Add Non-Volatile Storage APIs to ti.drivers| |TIDRIVERS-61|GPIOMSP430.h is missing __cpluspluss closing bracket| |TIDRIVERS-58|Concerto EMAC driver should signal NDK for link up/down status| |
Supported Operating Systems:
This release requires the following software components and tools versions to successfully function:
This release was validated using the following components:
IMPORTANT NOTICE ON CC1350 BLUETOOTH(R) SMART: This TI RTOS release contains a pre-release version of the Bluetooth Smart functionality in the (RF) radio driver for CC1350. The Bluetooth Smart API in the radio driver should not be used in production of CC1350-based products. The CC1350 production release Bluetooth Smart radio driver is in its final stages of development and verification, and it should be expected that radio-specific timings and parameters will change in that release. This notice does not apply to the Bluetooth Smart functionality in the radio driver for CC2640/50.
Please check the TI-RTOS Support Wiki for issues found after this product was released.
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 6.30.00.00-eng or 6.30.00.10-beta).
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory.
Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.
Last updated: February 25, 2016 Build Ver: 2.16.00.08