#include <rf_ble_cmd.h>
Data Fields | |
uint8_t | nTx |
uint8_t | nTxAck |
Total number of transmitted packets (including auto-empty) that have been ACK'ed. More... | |
uint8_t | nTxCtrl |
Number of unique LL control packets from the Tx queue that have been transmitted. More... | |
uint8_t | nTxCtrlAck |
Number of LL control packets from the Tx queue that have been finished (ACK'ed) More... | |
uint8_t | nTxCtrlAckAck |
uint8_t | nTxRetrans |
Number of retransmissions that has been done. More... | |
uint8_t | nTxEntryDone |
Number of packets from the Tx queue that have been finished (ACK'ed) More... | |
uint8_t | nRxOk |
Number of packets that have been received with payload, CRC OK and not ignored. More... | |
uint8_t | nRxCtrl |
Number of LL control packets that have been received with CRC OK and not ignored. More... | |
uint8_t | nRxCtrlAck |
uint8_t | nRxNok |
Number of packets that have been received with CRC error. More... | |
uint8_t | nRxIgnored |
uint8_t | nRxEmpty |
Number of packets that have been received with CRC OK and no payload. More... | |
uint8_t | nRxBufFull |
Number of packets that have been received and discarded due to lack of buffer space. More... | |
int8_t | lastRssi |
RSSI of last received packet. More... | |
struct { | |
uint8_t bTimeStampValid:1 | |
1 if a valid time stamp has been written to timeStamp; 0 otherwise More... | |
uint8_t bLastCrcErr:1 | |
1 if the last received packet had CRC error; 0 otherwise More... | |
uint8_t bLastIgnored:1 | |
1 if the last received packet with CRC OK was ignored; 0 otherwise More... | |
uint8_t bLastEmpty:1 | |
1 if the last received packet with CRC OK was empty; 0 otherwise More... | |
uint8_t bLastCtrl:1 | |
1 if the last received packet with CRC OK was empty; 0 otherwise More... | |
uint8_t bLastMd:1 | |
1 if the last received packet with CRC OK had MD = 1; 0 otherwise More... | |
uint8_t bLastAck:1 | |
} | pktStatus |
ratmr_t | timeStamp |
Slave operation: Time stamp of first received packet. More... | |
Definition at line 935 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::bLastAck |
1 if the last received packet with CRC OK was an ACK of a transmitted packet; 0 otherwise
Definition at line 962 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::bLastCrcErr |
1 if the last received packet had CRC error; 0 otherwise
Definition at line 957 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::bLastCtrl |
1 if the last received packet with CRC OK was empty; 0 otherwise
Definition at line 960 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::bLastEmpty |
1 if the last received packet with CRC OK was empty; 0 otherwise
Definition at line 959 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::bLastIgnored |
1 if the last received packet with CRC OK was ignored; 0 otherwise
Definition at line 958 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::bLastMd |
1 if the last received packet with CRC OK had MD = 1; 0 otherwise
Definition at line 961 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::bTimeStampValid |
1 if a valid time stamp has been written to timeStamp; 0 otherwise
Definition at line 956 of file rf_ble_cmd.h.
int8_t rfc_bleMasterSlaveOutput_s::lastRssi |
RSSI of last received packet.
Definition at line 954 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nRxBufFull |
Number of packets that have been received and discarded due to lack of buffer space.
Definition at line 953 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nRxCtrl |
Number of LL control packets that have been received with CRC OK and not ignored.
Definition at line 946 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nRxCtrlAck |
Number of LL control packets that have been received with CRC OK and not ignored, and then ACK'ed
Definition at line 947 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nRxEmpty |
Number of packets that have been received with CRC OK and no payload.
Definition at line 952 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nRxIgnored |
Number of packets that have been received with CRC OK and ignored due to repeated sequence number
Definition at line 950 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nRxNok |
Number of packets that have been received with CRC error.
Definition at line 949 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nRxOk |
Number of packets that have been received with payload, CRC OK and not ignored.
Definition at line 945 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nTx |
Total number of packets (including auto-empty and retransmissions) that have been transmitted
Definition at line 936 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nTxAck |
Total number of transmitted packets (including auto-empty) that have been ACK'ed.
Definition at line 938 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nTxCtrl |
Number of unique LL control packets from the Tx queue that have been transmitted.
Definition at line 939 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nTxCtrlAck |
Number of LL control packets from the Tx queue that have been finished (ACK'ed)
Definition at line 940 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nTxCtrlAckAck |
Number of LL control packets that have been ACK'ed and where an ACK has been sent in response
Definition at line 941 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nTxEntryDone |
Number of packets from the Tx queue that have been finished (ACK'ed)
Definition at line 944 of file rf_ble_cmd.h.
uint8_t rfc_bleMasterSlaveOutput_s::nTxRetrans |
Number of retransmissions that has been done.
Definition at line 943 of file rf_ble_cmd.h.
struct { ... } rfc_bleMasterSlaveOutput_s::pktStatus |
ratmr_t rfc_bleMasterSlaveOutput_s::timeStamp |
Slave operation: Time stamp of first received packet.
Definition at line 965 of file rf_ble_cmd.h.