#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0807. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
struct { | |
uint8_t bEnaFifo:1 | |
0: Do not enable FIFO in modem, so that received data is not available 1: Enable FIFO in modem – the data must be read out by the application More... | |
uint8_t bFsOff:1 | |
0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
uint8_t bNoSync:1 | |
0: Run sync search as normal for the configured mode 1: Write correlation thresholds to the maximum value to avoid getting sync More... | |
} | config |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger classifier for ending the operation. More... | |
uint32_t | syncWord |
Sync word to use for receiver. More... | |
ratmr_t | endTime |
Time to end the operation. More... | |
Definition at line 396 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_TEST_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 405 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_TEST_s::bEnaFifo |
0: Do not enable FIFO in modem, so that received data is not available
1: Enable FIFO in modem – the data must be read out by the application
Definition at line 416 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_TEST_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
Definition at line 418 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_TEST_s::bNoSync |
0: Run sync search as normal for the configured mode
1: Write correlation thresholds to the maximum value to avoid getting sync
Definition at line 420 of file rf_common_cmd.h.
uint16_t rfc_CMD_RX_TEST_s::commandNo |
The command ID number 0x0807.
Definition at line 397 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RX_TEST_s::condition |
struct { ... } rfc_CMD_RX_TEST_s::config |
ratmr_t rfc_CMD_RX_TEST_s::endTime |
Time to end the operation.
Definition at line 432 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RX_TEST_s::endTrigger |
Trigger classifier for ending the operation.
uint8_t rfc_CMD_RX_TEST_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 413 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_TEST_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 408 of file rf_common_cmd.h.
rfc_radioOp_t* rfc_CMD_RX_TEST_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 401 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_TEST_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 412 of file rf_common_cmd.h.
ratmr_t rfc_CMD_RX_TEST_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 402 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RX_TEST_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_RX_TEST_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 398 of file rf_common_cmd.h.
uint32_t rfc_CMD_RX_TEST_s::syncWord |
Sync word to use for receiver.
Definition at line 431 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_TEST_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 407 of file rf_common_cmd.h.
uint8_t rfc_CMD_RX_TEST_s::triggerType |
The type of trigger.
Definition at line 404 of file rf_common_cmd.h.