125 #ifndef ti_drivers_wifi_WiFiCC3100__include
126 #define ti_drivers_wifi_WiFiCC3100__include
132 #if defined(MSP430WARE)
133 #include <ti/sysbios/hal/Hwi.h>
135 #include <ti/sysbios/family/arm/m3/Hwi.h>
138 #include <ti/sysbios/knl/Semaphore.h>
uint32_t irqIntNum
Definition: WiFiCC3100.h:204
unsigned int spiIndex
Definition: WiFiCC3100.h:223
uint32_t enPort
Definition: WiFiCC3100.h:209
The definition of a WiFi function table that contains the required set of functions to control a spec...
Definition: WiFi.h:237
Definition: WiFiCC3100.h:152
void(* wifiIntFxn)()
Definition: WiFiCC3100.h:225
Definition: WiFiCC3100.h:150
struct WiFiCC3100_HWAttrs WiFiCC3100_HWAttrs
WiFiCC3100 Hardware attributes.
struct WiFiCC3100_Object WiFiCC3100_Object
WiFiCC3100 Object.
Semaphore_Struct readSemaphore
Definition: WiFiCC3100.h:227
Definition: WiFiCC3100.h:155
uint32_t csPin
Definition: WiFiCC3100.h:207
SPI Global configuration.
Definition: SPI.h:418
WiFiCC3100 Hardware attributes.
Definition: WiFiCC3100.h:201
Definition: WiFiCC3100.h:153
uint32_t bitRate
Definition: WiFiCC3100.h:222
volatile WiFiCC3100_SPI_State spiState
Definition: WiFiCC3100.h:230
uint32_t enPin
Definition: WiFiCC3100.h:210
bool isOpen
Definition: WiFiCC3100.h:232
uint32_t irqPort
Definition: WiFiCC3100.h:202
SPI_Handle spiHandle
Definition: WiFiCC3100.h:220
Definition: WiFiCC3100.h:151
WiFiCC3100 Object.
Definition: WiFiCC3100.h:218
Definition: WiFiCC3100.h:154
const WiFi_FxnTable WiFiCC3100_fxnTable
WiFi function table for CC3100 devices.
WiFiCC3100_SPI_State
SPI state machine. Not needed by user application.
Definition: WiFiCC3100.h:149
uint32_t irqPin
Definition: WiFiCC3100.h:203
Semaphore_Struct writeSemaphore
Definition: WiFiCC3100.h:228
Hwi_Struct wifiHwi
Definition: WiFiCC3100.h:219
uint32_t csPort
Definition: WiFiCC3100.h:206