47 #ifndef ti_drivers_uart_UARTCC3200DMA__include
48 #define ti_drivers_uart_UARTCC3200DMA__include
57 #include <ti/drivers/ports/ClockP.h>
58 #include <ti/drivers/ports/HwiP.h>
60 #include <ti/drivers/ports/SemaphoreP.h>
61 #include <ti/drivers/Power.h>
UART_STOP
UART stop bit settings.
Definition: UART.h:379
unsigned int readTimeout
Definition: UARTCC3200DMA.h:129
UART_Echo readEcho
Definition: UARTCC3200DMA.h:140
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:497
UART_PAR
UART parity type settings.
Definition: UART.h:389
UART_DataMode writeDataMode
Definition: UARTCC3200DMA.h:135
struct UARTCC3200DMA_Object UARTCC3200DMA_Object
UARTCC3200DMA Object.
UART_Mode
UART mode settings.
Definition: UART.h:291
UART_DataMode
UART data mode settings.
Definition: UART.h:339
struct UARTCC3200DMA_HWAttrs UARTCC3200DMA_HWAttrs
UARTCC3200DMA Hardware attributes.
UART_ReturnMode
UART return mode settings.
Definition: UART.h:324
Power_NotifyObj postNotify
Definition: UARTCC3200DMA.h:160
size_t readCount
Definition: UARTCC3200DMA.h:149
UART_Echo
UART echo settings.
Definition: UART.h:357
uint32_t baudRate
Definition: UARTCC3200DMA.h:136
UART_DataMode readDataMode
Definition: UARTCC3200DMA.h:134
ClockP_Handle txFifoEmptyClk
Definition: UARTCC3200DMA.h:159
SemaphoreP_Handle readSem
Definition: UARTCC3200DMA.h:154
size_t writeSize
Definition: UARTCC3200DMA.h:145
void * readBuf
Definition: UARTCC3200DMA.h:148
UART_Mode readMode
Definition: UARTCC3200DMA.h:127
unsigned int intNum
Definition: UARTCC3200DMA.h:110
UART_STOP stopBits
Definition: UARTCC3200DMA.h:138
SemaphoreP_Handle writeSem
Definition: UARTCC3200DMA.h:153
UART_LEN dataLength
Definition: UARTCC3200DMA.h:137
unsigned int intPriority
Definition: UARTCC3200DMA.h:112
const UART_FxnTable UARTCC3200DMA_fxnTable
const void * writeBuf
Definition: UARTCC3200DMA.h:143
void(* UART_Callback)(UART_Handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:284
UART_PAR parityType
Definition: UARTCC3200DMA.h:139
UARTCC3200DMA Hardware attributes.
Definition: UARTCC3200DMA.h:106
unsigned long rxChannelIndex
Definition: UARTCC3200DMA.h:114
unsigned int writeTimeout
Definition: UARTCC3200DMA.h:130
HwiP_Handle hwiHandle
Definition: UARTCC3200DMA.h:156
unsigned int baseAddr
Definition: UARTCC3200DMA.h:108
size_t readSize
Definition: UARTCC3200DMA.h:150
UART_LEN
UART data length settings.
Definition: UART.h:367
UART_Callback writeCallback
Definition: UARTCC3200DMA.h:132
size_t writeCount
Definition: UARTCC3200DMA.h:144
UART_ReturnMode readReturnMode
Definition: UARTCC3200DMA.h:133
UARTCC3200DMA Object.
Definition: UARTCC3200DMA.h:124
struct UARTCC3200DMA_Object * UARTCC3200DMA_Handle
UART_Callback readCallback
Definition: UARTCC3200DMA.h:131
unsigned long txChannelIndex
Definition: UARTCC3200DMA.h:116
bool opened
Definition: UARTCC3200DMA.h:126
UART_Mode writeMode
Definition: UARTCC3200DMA.h:128