50 #ifndef ti_drivers_emac_EMACSnow__include
51 #define ti_drivers_emac_EMACSnow__include
58 #include <ti/sysbios/knl/Swi.h>
59 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
60 #include <ti/sysbios/family/arm/m3/Hwi.h>
64 #ifndef _INCLUDE_NIMU_CODE
65 #define _INCLUDE_NIMU_CODE
67 #include <ti/ndk/inc/stkmain.h>
120 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
EMACSnow Hardware attributes.
Definition: EMACSnow.h:75
uint8_t * macAddress
Definition: EMACSnow.h:79
EMAC Function table structure.
Definition: EMAC.h:136
unsigned int intPriority
Definition: EMACSnow.h:78
unsigned int baseAddr
Definition: EMACSnow.h:76
struct EMACSnow_Object EMACSnow_Object
EMACSnow Object.
bool EMACSnow_isLinkUp(uint32_t index)
This function sets the EMACSnow driver.
unsigned int intNum
Definition: EMACSnow.h:77
int EMACSnow_NIMUInit(STKEVENT_Handle hEvent)
This function is needed in the NIMUDeviceTable that is required by the NDK.
Hwi_Handle hwi
Definition: EMACSnow.h:91
EMACSnow Object.
Definition: EMACSnow.h:89
Swi_Handle swi
Definition: EMACSnow.h:90
struct EMACSnow_HWAttrs EMACSnow_HWAttrs
EMACSnow Hardware attributes.
void EMACSnow_init(uint32_t index)
This function initializes the EMACSnow driver.
const EMAC_FxnTable EMACSnow_fxnTable
EMACSnow function table.