67 #ifndef ti_drivers_EMAC__include
68 #define ti_drivers_EMAC__include
88 #define EMAC_CMD_RESERVED 32
102 #define EMAC_STATUS_RESERVED -32
110 #define EMAC_STATUS_SUCCESS 0
118 #define EMAC_STATUS_ERROR -1
127 #define EMAC_STATUS_UNDEFINEDCMD -2
EMAC Function table structure.
Definition: EMAC.h:136
EMAC_FxnTable const * fxnTablePtr
Definition: EMAC.h:154
EMAC_InitFxn emacInit
Definition: EMAC.h:137
bool(* EMAC_isLinkUpFxn)(uint32_t)
Definition: EMAC.h:131
EMAC_isLinkUpFxn emacIsLinkUp
Definition: EMAC.h:138
void(* EMAC_InitFxn)(uint32_t)
Definition: EMAC.h:130
bool EMAC_isLinkUp(unsigned int index)
This function returns if the link is up.
void * object
Definition: EMAC.h:156
void EMAC_init(void)
This function initializes the EMAC driver.
struct EMAC_FxnTable EMAC_FxnTable
EMAC Function table structure.
struct EMAC_Config EMAC_Config
EMAC Global configuration.
void const * hwAttrs
Definition: EMAC.h:158
EMAC Global configuration.
Definition: EMAC.h:152