CC13xx Driver Library
[ddi] Digital to Digital Interface

Functions

static void AuxAdiDdiSafeWrite (uint32_t nAddr, uint32_t nData, uint32_t nSize)
 Safely write to AUX ADI/DDI interfaces using a semaphore. More...
 
static uint32_t AuxAdiDdiSafeRead (uint32_t nAddr, uint32_t nSize)
 Safely read from AUX ADI/DDI interfaces using a semaphore. More...
 
static void DDI32RegWrite (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
 Write a 32 bit value to a register in the DDI slave. More...
 
static uint32_t DDI32RegRead (uint32_t ui32Base, uint32_t ui32Reg)
 Read the value in a 32 bit register. More...
 
static void DDI32BitsSet (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
 Set specific bits in a DDI slave register. More...
 
static void DDI32BitsClear (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
 Clear specific bits in a 32 bit DDI register. More...
 
static void DDI8SetValBit (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Byte, uint16_t ui16Mask, uint16_t ui16Val)
 Set a value on any 8 bits inside a 32 bit register in the DDI slave. More...
 
static void DDI16SetValBit (uint32_t ui32Base, uint32_t ui32Reg, bool bWriteHigh, uint32_t ui32Mask, uint32_t ui32Val)
 Set a value on any 16 bits inside a 32 bit register aligned on a half-word boundary in the DDI slave. More...
 
void DDI16BitWrite (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32WrData)
 Write a single bit using a 16-bit maskable write. More...
 
void DDI16BitfieldWrite (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32Shift, uint16_t ui32Data)
 Write a bit field via the DDI using 16-bit maskable write. More...
 
uint16_t DDI16BitRead (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask)
 Read a bit via the DDI using 16-bit read. More...
 
uint16_t DDI16BitfieldRead (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32Shift)
 Read a bitfield via the DDI using 16-bit read. More...
 

Detailed Description

Function Documentation

static uint32_t AuxAdiDdiSafeRead ( uint32_t  nAddr,
uint32_t  nSize 
)
inlinestatic

Safely read from AUX ADI/DDI interfaces using a semaphore.

Note
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
nAddris the register address.
nSizeis the register access size in bytes.
Returns
Returns the data read.

Definition at line 168 of file ddi.h.

Referenced by ADI16RegRead(), ADI32RegRead(), ADI8RegRead(), ADIProtect(), DDI16BitfieldRead(), DDI16BitRead(), and DDI32RegRead().

Here is the call graph for this function:

static void AuxAdiDdiSafeWrite ( uint32_t  nAddr,
uint32_t  nData,
uint32_t  nSize 
)
inlinestatic

Safely write to AUX ADI/DDI interfaces using a semaphore.

Note
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
nAddris the register address.
nDatais the data to write to the register.
nSizeis the register access size in bytes.
Returns
None

Definition at line 136 of file ddi.h.

Referenced by ADI16BitsClear(), ADI16BitsSet(), ADI16RegWrite(), ADI16SetValBit(), ADI32BitsClear(), ADI32BitsSet(), ADI32RegWrite(), ADI4SetValBit(), ADI8BitsClear(), ADI8BitsSet(), ADI8RegWrite(), ADI8SetValBit(), ADIConfigSet(), ADIProtect(), ADISync(), DDI16BitfieldWrite(), DDI16BitWrite(), DDI16SetValBit(), DDI32BitsClear(), DDI32BitsSet(), DDI32RegWrite(), and DDI8SetValBit().

Here is the call graph for this function:

uint16_t DDI16BitfieldRead ( uint32_t  ui32Base,
uint32_t  ui32Reg,
uint32_t  ui32Mask,
uint32_t  ui32Shift 
)

Read a bitfield via the DDI using 16-bit read.

Requires that bit fields do not space the low/high word boundary.

Note
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
ui32Baseis the base address of the DDI port.
ui32Regis register to access.
ui32Maskis the mask defining which of the 16 bits that should be overwritten. The mask must be defined in the lower half of the 32 bits.
ui32Shiftdefines the required shift of the data to align with bit 0.
Returns
Returns data aligned to bit 0.

Definition at line 198 of file ddi.c.

Referenced by OSCClockSourceGet(), and OSCHfSourceReady().

Here is the call graph for this function:

void DDI16BitfieldWrite ( uint32_t  ui32Base,
uint32_t  ui32Reg,
uint32_t  ui32Mask,
uint32_t  ui32Shift,
uint16_t  ui32Data 
)

Write a bit field via the DDI using 16-bit maskable write.

Requires that bitfields not space the low/high word boundary.

Note
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
ui32Baseis the base address of the DDI port.
ui32Regis register to access.
ui32Maskis the mask defining which of the 16 bits that should be overwritten. The mask must be defined in the lower half of the 32 bits.
ui32Shift
ui32Data
Returns
None

Write a bit field via the DDI using 16-bit maskable write.

Definition at line 108 of file ddi.c.

Referenced by HapiTrimDeviceShutDown(), OSCClockLossEventDisable(), OSCClockLossEventEnable(), and OSCClockSourceSet().

Here is the call graph for this function:

uint16_t DDI16BitRead ( uint32_t  ui32Base,
uint32_t  ui32Reg,
uint32_t  ui32Mask 
)

Read a bit via the DDI using 16-bit read.

Note
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
ui32Baseis the base address of the DDI module.
ui32Regis the register to read.
ui32Maskdefines the bit which should be read.
Returns
Returns a zero if bit selected by mask is '0'. Else returns the mask.

Read a bit via the DDI using 16-bit read.

Definition at line 152 of file ddi.c.

Here is the call graph for this function:

void DDI16BitWrite ( uint32_t  ui32Base,
uint32_t  ui32Reg,
uint32_t  ui32Mask,
uint32_t  ui32WrData 
)

Write a single bit using a 16-bit maskable write.

A '1' is written to the bit if ui32WrData is non-zero, else a '0' is written.

Note
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
ui32Baseis the base address of the DDI port.
ui32Regis register to access.
ui32Maskis the mask defining which of the 16 bit that should be overwritten. The mask must be defined in the lower half of the 32 bits.
ui32WrDatais the value to write. The value must be defined in the lower half of the 32 bits.
Returns
None

Definition at line 64 of file ddi.c.

Referenced by OSCXHfPowerModeSet().

Here is the call graph for this function:

static void DDI16SetValBit ( uint32_t  ui32Base,
uint32_t  ui32Reg,
bool  bWriteHigh,
uint32_t  ui32Mask,
uint32_t  ui32Val 
)
inlinestatic

Set a value on any 16 bits inside a 32 bit register aligned on a half-word boundary in the DDI slave.

This function allows 16 bit masked access to the DDI slave registers.

Use this function to write any value in the range 0-15 bits aligned on a half-word boundary. Fx. for writing the value 0b101 to bits 1-3 set ui32Val = 0x000A and ui32Mask = 0x000E. Bits 0 and 5-15 will not be affected by the operation, as long as the corresponding bits are not set in the ui32Mask.

Note
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
ui32Baseis the base address of the DDI port.
ui32Regis register to access.
bWriteHighdefines which part of the register to write in.
ui32Maskis the mask defining which of the 16 bit that should be overwritten. The mask must be defined in the lower half of the 32 bits.
ui32Valis the value to write. The value must be defined in the lower half of the 32 bits.
Returns
None

Definition at line 448 of file ddi.h.

Here is the call graph for this function:

static void DDI32BitsClear ( uint32_t  ui32Base,
uint32_t  ui32Reg,
uint32_t  ui32Val 
)
inlinestatic

Clear specific bits in a 32 bit DDI register.

This function will clear bits in a register in the analog domain.

Note
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
ui32Baseis DDI base address.
ui32Regis the base registers to clear the bits in.
ui32Valis the 32 bit one-hot encoded value specifying which bits to clear in the register.
Returns
None

Definition at line 344 of file ddi.h.

Here is the call graph for this function:

static void DDI32BitsSet ( uint32_t  ui32Base,
uint32_t  ui32Reg,
uint32_t  ui32Val 
)
inlinestatic

Set specific bits in a DDI slave register.

This function will set bits in a register in the analog domain.

Note
This operation is write only for the specified register. This function is used to set bits in specific register in the DDI slave. Only bits in the selected register are affected by the operation.
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
ui32Baseis DDI base address.
ui32Regis the base register to assert the bits in.
ui32Valis the 32 bit one-hot encoded value specifying which bits to set in the register.
Returns
None

Definition at line 304 of file ddi.h.

Here is the call graph for this function:

static uint32_t DDI32RegRead ( uint32_t  ui32Base,
uint32_t  ui32Reg 
)
inlinestatic

Read the value in a 32 bit register.

This function will read a register in the analog domain and return the value as an uint32_t.

Note
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
ui32Baseis DDI base address.
ui32Regis the 32 bit register to read.
Returns
Returns the 32 bit value of the analog register.

Definition at line 267 of file ddi.h.

Here is the call graph for this function:

static void DDI32RegWrite ( uint32_t  ui32Base,
uint32_t  ui32Reg,
uint32_t  ui32Val 
)
inlinestatic

Write a 32 bit value to a register in the DDI slave.

This function will write a value to a register in the analog domain.

Note
This operation is write only for the specified register. No conservation of the previous value of the register will be kept (i.e. this is NOT read-modify-write on the register).
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
ui32Baseis DDI base address.
ui32Regis the register to write.
ui32Valis the 32 bit value to write to the register.
Returns
None

Definition at line 235 of file ddi.h.

Referenced by HapiTrimDeviceShutDown().

Here is the call graph for this function:

static void DDI8SetValBit ( uint32_t  ui32Base,
uint32_t  ui32Reg,
uint32_t  ui32Byte,
uint16_t  ui16Mask,
uint16_t  ui16Val 
)
inlinestatic

Set a value on any 8 bits inside a 32 bit register in the DDI slave.

This function allows byte (8 bit access) to the DDI slave registers.

Use this function to write any value in the range 0-7 bits aligned on a byte boundary. Fx. for writing the value 0b101 to bits 1-3 set ui16Val = 0x0A and ui16Mask = 0x0E. Bits 0 and 5-7 will not be affected by the operation, as long as the corresponding bits are not set in the ui16Mask.

Note
Both the AUX module and the clock for the AUX SMPH module must be enabled before calling this function.
Parameters
ui32Baseis the base address of the DDI port.
ui32Regis the Least Significant Register in the DDI slave that will be affected by the write operation.
ui32Byteis the byte number to access within the 32 bit register.
ui16Maskis the mask defining which of the 8 bits that should be overwritten. The mask must be defined in the lower half of the 16 bits.
ui16Valis the value to write. The value must be defined in the lower half of the 16 bits.
Returns
None

Definition at line 395 of file ddi.h.

Here is the call graph for this function:

Macro Definition Documentation

#define DDI_ACK   0x00000001

Definition at line 105 of file ddi.h.

#define DDI_PROTECT   0x00000080

Definition at line 104 of file ddi.h.

#define DDI_SLAVE_REGS   64
#define DDI_SYNC   0x00000000

Definition at line 106 of file ddi.h.