CC13xx Driver Library
adi.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_types.h>
#include <inc/hw_uart.h>
#include <inc/hw_memmap.h>
#include <inc/hw_ints.h>
#include <inc/hw_adi.h>
#include <driverlib/debug.h>
#include <driverlib/ddi.h>

Go to the source code of this file.

Macros

#define ADI_SLAVE_REGS   16
 
#define ADI_NO_WAIT   0x00000000
 
#define ADI_WAIT_FOR_ACK   0x00000004
 
#define ADI_SPEED_2   0x00000000
 
#define ADI_SPEED_4   0x00000001
 
#define ADI_SPEED_8   0x00000002
 
#define ADI_SPEED_16   0x00000003
 
#define ADI_CONFIG_MASK   0x00000007
 
#define ADI_PROTECT   0x00000080
 
#define ADI_ACK   0x00000001
 
#define ADI_SYNC   0x00000000
 

Functions

static uint32_t ADIStatusGet (uint32_t ui32Base)
 Get the status of an ADI module. More...
 
static void ADIConfigSet (uint32_t ui32Base, uint32_t ui32Config, bool bProtect)
 Configure the ADI Slave. More...
 
static void ADISync (uint32_t ui32Base)
 Synchronize the ADI slave. More...
 
static void ADIProtect (uint32_t ui32Base)
 Protect an ADI slave configuration by locking the configuration register access. More...
 
static void ADI8RegWrite (uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
 Write an 8 bit value to a register in an ADI slave. More...
 
static void ADI16RegWrite (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Val)
 Write a 16 bit value to 2 registers in the ADI slave. More...
 
static void ADI32RegWrite (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
 Write a 32 bit value to 4 registers in the ADI slave. More...
 
static uint32_t ADI8RegRead (uint32_t ui32Base, uint32_t ui32Reg)
 Read the value of an 8 bit register in the ADI slave. More...
 
static uint32_t ADI16RegRead (uint32_t ui32Base, uint32_t ui32Reg)
 Read the value in a 16 bit register. More...
 
static uint32_t ADI32RegRead (uint32_t ui32Base, uint32_t ui32Reg)
 Read the value in a 32 bit register. More...
 
static void ADI8BitsSet (uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
 Set specific bits in a single 8 bit ADI register. More...
 
static void ADI16BitsSet (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Val)
 Set specific bits in 2 x 8 bit ADI slave registers. More...
 
static void ADI32BitsSet (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
 Set specific bits in 4 x 8 bit ADI slave registers. More...
 
static void ADI8BitsClear (uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
 Clear specific bits in an 8 bit ADI register. More...
 
static void ADI16BitsClear (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Val)
 Clear specific bits in two 8 bit ADI register. More...
 
static void ADI32BitsClear (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
 Clear specific bits in four 8 bit ADI register. More...
 
static void ADI4SetValBit (uint32_t ui32Base, uint32_t ui32Reg, bool bWriteHigh, uint8_t ui8Mask, uint8_t ui8Val)
 Set a value on any 4 bits inside an 8 bit register in the ADI slave. More...
 
static void ADI8SetValBit (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Mask, uint16_t ui16Val)
 Set a value on any bits inside an 8 bit register in the ADI slave. More...
 
static void ADI16SetValBit (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32Val)
 Set a value on any bits inside an 2 x 8 bit register aligned on a half-word (byte) boundary in the ADI slave. More...