TI-RTOS for SimpleLink Wireless MCUs  2.14.01.20
Data Structures | Macros | Typedefs | Enumerations | Variables
I2CCC26XX.h File Reference

Detailed Description

I2C driver implementation for a CC26XX I2C controller.

============================================================================

Driver Include

The I2C header file should be included in an application as follows:

Overview

The general I2C API is normally used in application code, e.g. I2C_open() is used instead of I2CCC26XX_open(). The board file will define the device specific config, and casting in the general API will ensure that the correct device specific functions are called. This is also reflected in the example code in Use Cases.

General Behavior

Before using the I2C in CC26XX:

The following is true for receive operation:

The following apply for transmit operation:

After I2C operation has ended:

Error handling

If an error occurs during operation:

Power Management

The I2CCC26XX driver is setting a power constraint during operation to keep the device out of standby, i.e. device will enter idle mode when no tasks are active. When the operation has finished, the power constraint is released. The following statements are valid:

Supported Functions

Generic API Function API Function Description
I2C_init() I2CCC26XX_init() Initialize I2C driver
I2C_open() I2CCC26XX_open() Initialize I2C HW and set system dependencies
I2C_close() I2CCC26XX_close() Disable I2C HW and release system dependencies
I2C_transfer() I2CCC26XX_transfer() Start I2C transfer
Note
All calls should go through the generic API.

Unsupported Functionality

The CC26XX I2C driver currently does not support:

Use Cases

Basic Receive

Receive 10 bytes over I2C in I2C_MODE_BLOCKING.

// Locals
I2C_Handle handle;
I2C_Params params;
I2C_Transaction i2cTrans;
uint8_t rxBuf[32]; // Receive buffer
uint8_t txBuf[32]; // Transmit buffer
// Configure I2C parameters.
I2C_Params_init(&params);
// Initialize master I2C transaction structure
i2cTrans.writeCount = 0;
i2cTrans.writeBuf = txBuf;
i2cTrans.readCount = 10;
i2cTrans.readBuf = rxBuf;
i2cTrans.slaveAddress = 0x3C;
// Open I2C
handle = I2C_open(Board_I2C, &params);
// Do I2C transfer receive
I2C_transfer(handle, &i2cTrans);

Basic Transmit

Transmit 16 bytes over I2C in I2C_MODE_CALLBACK.

uint8_t rxBuffer[32]; // Receive buffer
uint8_t txBuffer[32]; // Transmit buffer
bool transferDone = false;
static void transferCallback(I2C_Handle handle, I2C_Transaction *transac, bool result)
{
// Set length bytes
if (result) {
transferDone = true;
} else {
// Transaction failed, act accordingly...
.
.
}
}
static void taskFxn(UArg a0, UArg a1)
{
// Locals
I2C_Handle handle;
I2C_Params params;
I2C_Transaction i2cTrans;
// Configure I2C parameters.
I2C_Params_init(&params);
params.transferCallbackFxn = transferCallback;
// Prepare data to send, send 0x00, 0x01, 0x02, ...0xFF, 0x00, 0x01...
for(uint32_t i = 0; i < numTxBytes; i++)
txBuffer[i] = (uint8_t) i;
// Initialize master I2C transaction structure
i2cTrans.writeCount = 16;
i2cTrans.writeBuf = txBuffer;
i2cTrans.readCount = 0;
i2cTrans.readBuf = rxBuffer;
i2cTrans.slaveAddress = 0x3C;
// Open I2C
handle = I2C_open(Board_I2C, &params);
// Do I2C transfer (in callback mode)
I2C_transfer(handle, &i2cTrans);
// Do other stuff while I2C is handling the transfer
.
.
// Do something if I2C transfer is finished
if(transferDone) {
.
.
}
// Continue...
.
.
}

Chained Transactions

Transmit 10 bytes and then 32 bytes over I2C in I2C_MODE_CALLBACK.

uint8_t rxBuffer[32]; // Receive buffer
uint8_t txBuffer[32]; // Transmit buffer
uint8_t rxBuffer2[64]; // 2. Receive buffer
uint8_t txBuffer2[64]; // 2. Transmit buffer
bool transferDone = false;
static void writeCallbackDefault(I2C_Handle handle, I2C_Transaction *transac, bool result)
{
// Set length bytes
if (result) {
transferDone = true;
} else {
// Transaction failed, act accordingly...
.
.
}
}
static void taskFxn(UArg a0, UArg a1)
{
// Locals
I2C_Handle handle;
I2C_Params params;
I2C_Transaction i2cTrans;
I2C_Transaction i2cTrans2;
// Configure I2C parameters.
I2C_Params_init(&params);
params.transferCallbackFxn = writeCallbackDefault;
// Prepare data to send, send 0x00, 0x01, 0x02, ...0xFF, 0x00, 0x01...
for(uint32_t i = 0; i < numTxBytes; i++)
txBuffer[i] = (uint8_t) i;
// Initialize first master I2C transaction structure
i2cTrans.writeCount = 10;
i2cTrans.writeBuf = txBuffer;
i2cTrans.readCount = 0;
i2cTrans.readBuf = rxBuffer;
i2cTrans.slaveAddress = 0x3C;
// Second transaction
i2cTrans2.writeCount = 32;
i2cTrans2.writeBuf = txBuffer2;
i2cTrans2.readCount = 0;
i2cTrans2.readBuf = rxBuffer2;
i2cTrans2.slaveAddress = 0x2E;
// Open I2C
handle = I2C_open(Board_I2C, &params);
// Do chained I2C transfers (in callback mode).
I2C_transfer(handle, &i2cTrans);
I2C_transfer(handle, &i2cTrans2);
// Do other stuff while I2C is handling the transfers
.
.
// Do something if I2C transfers are finished
if(transferDone) {
.
.
}
// Continue...
.
.
}

Instrumentation

The I2C driver interface produces log statements if instrumentation is enabled.

Diagnostics Mask Log details
Diags_USER1 basic I2C operations performed
Diags_USER2 detailed I2C operations performed

#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/I2C.h>
#include <ti/drivers/pin/PINCC26XX.h>
#include <ti/sysbios/family/arm/cc26xx/Power.h>
#include <ti/sysbios/family/arm/m3/Hwi.h>
#include <ti/sysbios/knl/Semaphore.h>
Include dependency graph for I2CCC26XX.h:

Go to the source code of this file.

Data Structures

struct  I2CCC26XX_I2CPinCfg
 I2CCC26XX Pin Configuration. More...
 
struct  I2CCC26XX_HWAttrs
 I2CCC26XX Hardware attributes. More...
 
struct  I2CCC26XX_Object
 I2CCC26XX Object. More...
 

Macros

#define ti_sysbios_family_arm_m3_Hwi__nolocalnames
 

Typedefs

typedef unsigned long I2CBaseAddrType
 
typedef unsigned long I2CDataType
 
typedef struct I2CCC26XX_I2CPinCfg I2CCC26XX_I2CPinCfg
 I2CCC26XX Pin Configuration. More...
 
typedef enum I2CCC26XX_Mode I2CCC26XX_Mode
 I2CCC26XX mode. More...
 
typedef struct I2CCC26XX_HWAttrs I2CCC26XX_HWAttrs
 I2CCC26XX Hardware attributes. More...
 
typedef struct I2CCC26XX_Object I2CCC26XX_Object
 I2CCC26XX Object. More...
 

Enumerations

enum  I2CCC26XX_Mode {
  I2CCC26XX_IDLE_MODE = 0,
  I2CCC26XX_WRITE_MODE,
  I2CCC26XX_READ_MODE,
  I2CCC26XX_ERROR = 0xFF
}
 I2CCC26XX mode. More...
 

Variables

const I2C_FxnTable I2CCC26XX_fxnTable
 

Macro Definition Documentation

#define ti_sysbios_family_arm_m3_Hwi__nolocalnames

Typedef Documentation

typedef unsigned long I2CBaseAddrType

I2C Base Address type.

typedef unsigned long I2CDataType

I2CCC26XX Pin Configuration.

Pin configuration that holds non-default pins. The default pin configuration is typically defined in I2CCC26XX_HWAttrs placed in the board file. The pin configuration structure is used by setting the custom void pointer in the I2C_Params to point to this struct. If the custom void pointer is NULL, the I2CCC26XX_HWAttrs pin mapping will be used.

1 I2C_Handle handle;
2 I2C_Params i2cParams;
3 I2CCC26XX_I2CPinCfg pinCfg;
4 
5 I2C_Params_init(&i2cParams); // sets custom to NULL
6 pinCfg.pinSDA = Board_I2C0_SDA1;
7 pinCfg.pinSCL = Board_I2C0_SCL1;
8 i2cParams.custom = &pinCfg;
9 
10 handle = I2C_open(Board_I2C, &i2cParams);

I2CCC26XX mode.

This enum defines the state of the I2C driver's state-machine. Do not modify.

I2CCC26XX Hardware attributes.

These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For cc26xxware these definitions are found in:

  • inc/hw_memmap.h
  • inc/hw_ints.h

A sample structure is shown below:

1 const I2CCC26XX_HWAttrs i2cCC26XXHWAttrs[] = {
2  {
3  .baseAddr = I2C0_BASE,
4  .powerMngrId = PERIPH_I2C0,
5  .intNum = INT_I2C,
6  .intPriority = (~0),
7  .sdaPin = Board_I2C_SDA,
8  .sclPin = Board_I2C_SCL,
9  },
10 };

I2CCC26XX Object.

The application must not access any member variables of this structure!

Enumeration Type Documentation

I2CCC26XX mode.

This enum defines the state of the I2C driver's state-machine. Do not modify.

Enumerator
I2CCC26XX_IDLE_MODE 
I2CCC26XX_WRITE_MODE 
I2CCC26XX_READ_MODE 
I2CCC26XX_ERROR 

Variable Documentation

const I2C_FxnTable I2CCC26XX_fxnTable
Copyright 2015, Texas Instruments Incorporated