SysLink API Reference
2.21.00.03
|
This file contains APIs and defines that are used by applications only on the host-side of the device.
Go to the source code of this file.
Data Structures | |
struct | Ipc_Terminate |
Argument for the Ipc_CONTROLCMD_SETTERMINATEPOLICY command. More... |
Macros | |
#define | Ipc_TERMINATEPOLICY_STOP 1 |
Use the stop terminate policy. | |
#define | Ipc_TERMINATEPOLICY_NOTIFY 2 |
Use the notify terminate policy. | |
#define | Ipc_CONTROLCMD_LOADCALLBACK (0xBABE0000) |
Control command ID for load callback. | |
#define | Ipc_CONTROLCMD_STARTCALLBACK (0xBABE0001) |
Control command ID for start callback. | |
#define | Ipc_CONTROLCMD_STOPCALLBACK (0xBABE0002) |
Control command ID for stop callback. | |
#define | Ipc_CONTROLCMD_SETTERMINATEPOLICY (0xBABE0003) |
Control command ID for specifying the terminate handling policy. |
Functions | |
Int | Ipc_control (UInt16 procId, Int32 cmdId, Ptr arg) |
Perform IPC-related control operations with a specific slave. | |
Int | Ipc_runtimeId (UInt8 *rtid) |
Return a runtime id for the given application key. |
#define Ipc_TERMINATEPOLICY_STOP 1 |
Use the stop terminate policy.
When the host process termiantes (e.g. CTRL-C, SIGKILL), this terminate policy will stop the remote processor and place it into reset. The terminate action is carried out by the SysLink driver on behalf of the terminated process.
#define Ipc_TERMINATEPOLICY_NOTIFY 2 |
Use the notify terminate policy.
When the host process termiantes (e.g. CTRL-C, SIGKILL), this terminate policy will send a notify event to the remote processor. The lineId and eventId are determined by the remote executable through configuration parameters (See ti/syslink/ipc/rtos/SysLink.xdc).
#define Ipc_CONTROLCMD_LOADCALLBACK (0xBABE0000) |
Control command ID for load callback.
This command must be sent (via Ipc_control()) before using IPC with the slave, and after loading the slave.
This call ensures resources (e.g. Shared Region 0) are visible to the slave (for example, by enabling the slave-side MMU). This call then typically enables the slave-side call to Ipc_start() to succeed.
When ProcMgr is used to load the slave (the typical case), the arg
passed to Ipc_control() should be NULL.
When ProcMgr is not used to load the slave (supported, but not the typical case), the arg
passed to Ipc_control() must be a pointer to the slave-side address of the _Ipc_ResetVector
symbol. This is often obtained by inspecting the slave-side executable's .map file.
#define Ipc_CONTROLCMD_STARTCALLBACK (0xBABE0001) |
Control command ID for start callback.
This command must be sent (via Ipc_control()) before using IPC with the slave, and after sending the Ipc_CONTROLCMD_LOADCALLBACK command.
This call performs a handshake with the slave processor, typically enabling the slave-side call to Ipc_attach() to succeed.
When sending this command, the arg
passed to Ipc_control() should be NULL.
#define Ipc_CONTROLCMD_STOPCALLBACK (0xBABE0002) |
Control command ID for stop callback.
This command must be sent (via Ipc_control()) to detach from an attached slave.
This call first performs a handshake with the slave processor, typically enabling the slave-side calls to Ipc_detach() and Ipc_stop() to succeed. It then may make resources (e.g. Shared Region 0) inaccessible to the slave (for example by disabling the slave's MMU).
When ProcMgr is used to load the slave (the typical case), the arg
passed to Ipc_control() should be NULL.
When ProcMgr is not used to load the slave (supported, but not the typical case), the arg
passed to Ipc_control() must be a pointer to the slave-side address of the _Ipc_ResetVector
symbol. This is often obtained by inspecting the slave-side executable's .map file.
#define Ipc_CONTROLCMD_SETTERMINATEPOLICY (0xBABE0003) |
Control command ID for specifying the terminate handling policy.
Specify the terminate policy to be used by SysLink in the event that the application terminates. The SysLink driver will perform the requested terminate actions on behalf of the terminated application. This is typically used to handle cleanup of resources.
The arg
passed to Ipc_control() must be pointer to an Ipc_Terminate structure.
Perform IPC-related control operations with a specific slave.
[in] | procId | Remote processor ID |
[in] | cmdId | Command ID |
[in] | arg | Argument. The value of arg depends on the command being sent in cmdId . |
cmdId
describes its usage of the arg
param.Return a runtime id for the given application key.
When the application calls SysLink_setup(), there is an internal runtime id assigned to the application's process id. Use this API to retrieve the assigned runtime id. This API may be called multiple times but will always return the same runtime id for the current process id. This ensures that all levels of the software stack will be assigned the same runtime id.
There are 255 available runtime ids: 1 - 255. Runtime ids are allocated by looking for the next larger unused runtime id. The search will wrap around as needed.
[out] | rtid | Remote processor ID |
Ipc_S_SUCCESS | Operation succeeded |
Ipc_E_FAIL | No more runtime ids available |