Header file implementing Memory manager. It is a wrapper implementation to support Shared memory allocation using heap address translations using shared region or Tiler buffer allocation using tiler buffer manager and address translations.
Data Structures |
struct | SyslinkMemMgr_CreateParams_tag |
| Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params. More...
|
struct | SyslinkMemMgr_AllocBlock_tag |
struct | SyslinkMemMgr_AllocParams_tag |
| Alloc params. More...
|
Defines |
#define | MEMMGR_MAX_NAME_LENGTH 32u |
#define | MEMMGR_MAX_TILER_BLOCKS 10u |
#define | SyslinkMemMgr_Params SyslinkMemMgr_CreateParams |
Typedefs |
typedef enum
SyslinkMemMgr_Type_Type_tag | SyslinkMemMgr_Type |
| enum for denoting the different types of SyslinkMemMgr implementations.
|
typedef struct
SyslinkMemMgr_CreateParams_tag | SyslinkMemMgr_CreateParams |
| Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params.
|
typedef struct
SyslinkMemMgr_AllocBlock_tag | SyslinkMemMgr_AllocBlock |
typedef struct
SyslinkMemMgr_AllocParams_tag | SyslinkMemMgr_AllocParams |
| Alloc params.
|
typedef struct SyslinkMemMgr_Object | SyslinkMemMgr_Object |
| Forward declaration of structure defining object for the MemoryManger.
|
typedef SyslinkMemMgr_Object * | SyslinkMemMgr_Handle |
| Handle for the MemoryManager instance.
|
Enumerations |
enum | SyslinkMemMgr_AddrType {
SyslinkMemMgr_AddrType_Virtual = 0u,
SyslinkMemMgr_AddrType_Portable = 1u,
SyslinkMemMgr_AddrType_EndValue = 2u
} |
| Enumerations to indicate address types used for translation.
More...
|
enum | SyslinkMemMgr_Type_Type_tag {
SyslinkMemMgr_TYPE_SHAREDMEM = 0x0,
SyslinkMemMgr_TYPE_TILERMEM = 0x1
} |
| enum for denoting the different types of SyslinkMemMgr implementations.
More...
|
Functions |
Int32 | SyslinkMemMgr_setup (Void) |
Int32 | SyslinkMemMgr_destroy (Void) |
SyslinkMemMgr_Handle | SyslinkMemMgr_create (Ptr params) |
Int32 | SyslinkMemMgr_delete (SyslinkMemMgr_Handle *pHandle) |
Ptr | SyslinkMemMgr_alloc (SyslinkMemMgr_Handle handle, SyslinkMemMgr_AllocParams *params) |
Int32 | SyslinkMemMgr_free (SyslinkMemMgr_Handle handle, Ptr ptr, UInt32 size) |
Ptr | SyslinkMemMgr_map (SyslinkMemMgr_Handle handle, Ptr arg) |
Int32 | SyslinkMemMgr_unmap (SyslinkMemMgr_Handle handle, Ptr arg) |
Ptr | SyslinkMemMgr_translate (SyslinkMemMgr_Handle handle, Ptr srcAddr, SyslinkMemMgr_AddrType srcAddrType, SyslinkMemMgr_AddrType desAddrType) |
Ptr | SyslinkMemMgr_getKnlHandle (SyslinkMemMgr_Handle handle) |