Defines | Enumerations | Functions

Cache.h File Reference


Detailed Description

Defines Cache API interface.

Go to the source code of this file.

Defines

#define Cache_S_ALREADYSETUP   (1)
 Cache module is already setup.
#define Cache_S_SUCCESS   (0)
 Operation is successful.
#define Cache_E_FAIL   (-1)
 Generic failure.
#define Cache_E_INVALIDARG   (-2)
 Argument passed to a function is invalid.
#define Cache_E_OSFAILURE   (-3)
 Failure in OS call.

Enumerations

enum  Cache_Type {
  Cache_Type_L1P = 0x1,
  Cache_Type_L1D = 0x2,
  Cache_Type_L1 = 0x3,
  Cache_Type_L2P = 0x4,
  Cache_Type_L2D = 0x8,
  Cache_Type_L2 = 0xC,
  Cache_Type_ALL = 0xffff
}
enum  Cache_Mode {
  Cache_Mode_FREEZE,
  Cache_Mode_BYPASS,
  Cache_Mode_NORMAL
}

Functions

Void Cache_inv (Ptr blockPtr, UInt32 byteCnt, Bits16 type, Bool wait)
 Invalidate the Cache module.
Void Cache_wb (Ptr blockPtr, UInt32 byteCnt, Bits16 type, Bool wait)
 Writeback the Cache module.
Void Cache_wbInv (Ptr blockPtr, UInt32 byteCnt, Bits16 type, Bool wait)
 Write Back and Invalidate the Cache module.
Void Cache_wait (Void)
 Wait for cache operation to complete.
enum Cache_Mode Cache_setMode (Bits16 type, enum Cache_Mode mode)
 Set the mode of Cache module.

Define Documentation

#define Cache_S_ALREADYSETUP   (1)

Cache module is already setup.

#define Cache_S_SUCCESS   (0)

Operation is successful.

#define Cache_E_FAIL   (-1)

Generic failure.

#define Cache_E_INVALIDARG   (-2)

Argument passed to a function is invalid.

#define Cache_E_OSFAILURE   (-3)

Failure in OS call.


Enumeration Type Documentation

enum Cache_Type

Lists of bitmask cache types

Enumerator:
Cache_Type_L1P 
Cache_Type_L1D 

Level 1 Program cache

Cache_Type_L1 

Level 1 Data cache

Cache_Type_L2P 

Level 1 caches

Cache_Type_L2D 

Level 2 Program cache

Cache_Type_L2 

Level 2 Data cache

Cache_Type_ALL 

Level 2 caches

enum Cache_Mode

Lists of cache modes

Enumerator:
Cache_Mode_FREEZE 
Cache_Mode_BYPASS 
Cache_Mode_NORMAL 

Function Documentation

Void Cache_inv ( Ptr  blockPtr,
UInt32  byteCnt,
Bits16  type,
Bool  wait 
)

Invalidate the Cache module.

See also:
Cache_inv
Void Cache_wb ( Ptr  blockPtr,
UInt32  byteCnt,
Bits16  type,
Bool  wait 
)

Writeback the Cache module.

See also:
Cache_wb
Void Cache_wbInv ( Ptr  blockPtr,
UInt32  byteCnt,
Bits16  type,
Bool  wait 
)

Write Back and Invalidate the Cache module.

See also:
Cache_wbInv
Void Cache_wait ( Void   )

Wait for cache operation to complete.

See also:
Cache_wait
enum Cache_Mode Cache_setMode ( Bits16  type,
enum Cache_Mode  mode 
)

Set the mode of Cache module.

See also:
Cache_setMode
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated