Cache interface definitions for QNX.
#include <sys/cache.h>
#include <ti/syslink/inc/Bitops.h>
#include <ti/syslink/utils/Cache.h>
Go to the source code of this file.
Data Structures | |
struct | Cache_ModuleObject |
Structure defining state object of cache module. More... | |
Typedefs | |
typedef struct Cache_ModuleObject | Cache_ModuleObject |
Structure defining state object of cache module. | |
Functions | |
Int32 | Cache_setup (void) |
Int32 | Cache_destroy (void) |
typedef struct Cache_ModuleObject Cache_ModuleObject |
Structure defining state object of cache module.
Int32 Cache_setup | ( | void | ) |
Int32 Cache_destroy | ( | void | ) |