Defines configurable elements for FrameQ module.
Go to the source code of this file.
Data Structures | |
struct | Frame_FrameBufInfo_tag |
Structure to frame buffer informantion in frame header. More... | |
struct | Frame_FrameHeader_Tag |
Structure of the base frame header. FrameQ maintains list of frames to be retrieved by FrameQ reader client. Application is expected to use Helper API to extract fileds and exteneded header pointer. More... | |
Defines | |
#define | FrameQ_MAX_FRAMESINVAPI (64u) |
Macro used in FrameQ for sorting of passed parameters in V API. In FrameQ_allocv case this denotes the number of frames that can be allocated in one call. In FrameQ_putv case this denotes the number of frames that can be put in one call. In FrameQ_getv case this denotes the number of frames that can be retrieved in one call. | |
Typedefs | |
typedef struct Frame_FrameBufInfo_tag | Frame_FrameBufInfo |
Structure to frame buffer informantion in frame header. | |
typedef struct Frame_FrameHeader_Tag | Frame_FrameHeader |
Structure of the base frame header. FrameQ maintains list of frames to be retrieved by FrameQ reader client. Application is expected to use Helper API to extract fileds and exteneded header pointer. | |
typedef Frame_FrameHeader * | Frame |
Defines the type for a frame pointer. |
#define FrameQ_MAX_FRAMESINVAPI (64u) |
Macro used in FrameQ for sorting of passed parameters in V API. In FrameQ_allocv case this denotes the number of frames that can be allocated in one call. In FrameQ_putv case this denotes the number of frames that can be put in one call. In FrameQ_getv case this denotes the number of frames that can be retrieved in one call.
typedef struct Frame_FrameBufInfo_tag Frame_FrameBufInfo |
Structure to frame buffer informantion in frame header.
typedef struct Frame_FrameHeader_Tag Frame_FrameHeader |
Structure of the base frame header. FrameQ maintains list of frames to be retrieved by FrameQ reader client. Application is expected to use Helper API to extract fileds and exteneded header pointer.
typedef Frame_FrameHeader* Frame |
Defines the type for a frame pointer.